Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Hi,
I have some problems with mDDR in secure device on secure kernel mode.
I do the folloing tests:(My dsp ubl just initialize ddr, and do some write and read test)
step1:
I configure the ini file to configure DSP core uses non-secure kernel mode. At this situation, program works well.
And the Hardware Security Controller registers' value:
scmmRegs->PID = 0x44842a00
scmmRegs->SYSSTATUS = 0x903a2
scmmRegs->SYSWR = 0x1
scmmRegs->SYSCONTROL = 0x0
scmmRegs->SYSCONTROLPROTECT = 0x20000
scmmRegs->SYSTAPEN = 0xffffffff
scmmRegs->SECRESERVED = 0x13
step2:
I change the ini file to configure DSP core uses secure kernel mode. At this situation, ddr2 controller is initialized well.
(I compare the registers' value both non-secure and secure kernel, they are same.)
But when program read/write the ddr, program counter run away.
And the Hardware Security Controller registers' value:
scmmRegs->PID = 0x44842a00
scmmRegs->SYSSTATUS = 0x80080302
scmmRegs->SYSWR = 0x0
scmmRegs->SYSCONTROL = 0x0
scmmRegs->SYSCONTROLPROTECT = 0x80
scmmRegs->SYSTAPEN = 0xffffffff
scmmRegs->SECRESERVED = 0x13
Difference between non-secure and secure of Hardware Security Controller registers' value are:
scmmRegs->SYSSTATUS = 0x903a2(non-secure) scmmRegs->SYSSTATUS = 0x80080302(secure)
scmmRegs->SYSWR = 0x1 (non-secure) scmmRegs->SYSWR = 0x0(non-secure)
scmmRegs->SYSCONTROLPROTECT = 0x20000 scmmRegs->SYSCONTROLPROTECT = 0x80
Refer to section 2.5.5 in OMAPL138_C6748_Generic_Security_Users_Guide_v1.0.2 and Memory_Protection_03_2012_v01
there are some resources restricted. Furthermore, refer to URL:
http://processors.wiki.ti.com/index.php/Basic_Secure_Boot_for_OMAP-L138_C6748#What_is_the_preferred_method_of_flashing_a_secure_device.3F
; This section allows configuration of one the systme IOPUs.
; The iopuNum field must be valid (0-5) and then mppaStart
; and mppaend fields allow setting a range of mppa MMRs to the
; same supplied mppa value.
; IOPUSELECT: | RSVD | iopuNum| mppaStart | mppaEnd |
; MPPAVALUE: | mppaValue |
The value of iopuNum can be (0~5), and refter to IOPU_Users_Guide, There is only 0~3. So what are others two used for?
Could some one provide any detail documentens relate to these(MPU and IOPUs).
Thanks!
Follwing contents is my ini file works for above test:
;***************************************************************
; TI OMAP-L138 / C6748 Security Utilities *
; (C) 2009-2012 Texas Instruments, Inc. *
;***************************************************************
;
; This INI file will create a header that contains:
; NOR config word (1 word)
; AIS magic number (1 word)
; AIS key load command (1 word)
; AIS key header (8 words)
; AIS set exit type (2 words)
; AIS set command + params (5 words)
; Signature (16 words)
;
; The AIS set command at the bottom of the INI file is a dummy write
; in order to force a signature check. This is necessary in order to
; create a well defined header that can be bound to the device. If
; the AIS set command is not used, then you will have to determine
; where the first signature occurs so that you can bind the entire
; section.
;
; *********************** INI ************************
; General settings that can be overwritten in the host code
; that calls the AISGen library.
[General]
; Can be 8 or 16 - used in emifa
busWidth=16
; SPIMASTER,I2CMASTER,EMIFA,NAND,EMAC,UART,PCI,HPI,USB,MMC_SD,VLYNQ,RAW
BootMode=EMIFA
; NO_CRC,SECTION_CRC,SINGLE_CRC
crcCheckType=NO_CRC
; Security settings (keys, options, list of sections to encrypt, etc.)
[Security]
; Security Type: GENERIC, CUSTOM, NONE
securityType=GENERIC
; Boot Exit Type: NONSECURE, SECUREWITHSK
; NONSECURE = Device switches from secure type to non-secure type, jumping to loaded code
; (no secure kernel since no longer secure device).
; SECUREWITHSK = Device remains as secure type, secure kernel is loaded, allowing run-time
; security context switching.
; for secure mode test
bootExitType = SECUREWITHSK
; for non-secure mode test
;bootExitType = NONSECURE
; Encrypt section list (ALL or comma-separated list of section names)
encryptSections=ALL
; CEK used for AES encryption of data - must be string of 32 hexadecimal characters
; Device uses KEK to encrypt CEK, and then SECURE KEY LOAD command load this CEK, uses to
; decrypt the data by ENCRYPTED SECTION LOAD command
;encryptionKey=4A7E1F56AE545D487C452388A65B0C05
encryptionKey=0123456789abcdeffedcba9876543210
; SHA Algorithm Selection
genericSHASelection = SHA1
; This section allows configuration of one the systme IOPUs.
; The iopuNum field must be valid (0-5) and then mppaStart
; and mppaend fields allow setting a range of mppa MMRs to the
; same supplied mppa value.
; IOPUSELECT: | RSVD | iopuNum| mppaStart | mppaEnd |
; MPPAVALUE: | mppaValue |
[IOPUCONFIG]
IOPUSELECT = 0x000000FF
MPPAVALUE = 0xFFFFFFFF
[IOPUCONFIG]
IOPUSELECT = 0x000100FF
MPPAVALUE = 0xFFFFFFFF
[IOPUCONFIG]
IOPUSELECT = 0x000200FF
MPPAVALUE = 0xFFFFFFFF
[IOPUCONFIG]
IOPUSELECT = 0x000300FF
MPPAVALUE = 0xFFFFFFFF
;This will set all security bits in IOPU6 registers to unlock security
;protection on all IOs protected but will lock the SYCFG registers to
;access only by secure supervisor ROM or secure kernel.
[IOPUCONFIG]
IOPUSELECT = 0x000600FF
MPPAVALUE = 0xFFFFFFFF
;This will set bit 7 of IOPU6 to 0 that will unlock the security protection
;on SYSCFG registers which is ideally what you need to configure PINMUX and
;other system registers.
[IOPUCONFIG]
IOPUSELECT = 0x00060707
MPPAVALUE = 0x00000000
; This section allow setting the MPU1 or MPU2. If the
; rangenum is out of the allowed range then all the ranges
; (including the fixed range) take the start, end, and
; protection values.
; |------24|------16|----------8|----------0|
; MPUSELECT: | RSVD | mpuNum | rangeNum |
; STARTADDR: | startAddr |
; ENDADDR: | endAddr |
; MPPAVALUE: | mppaValue |
[MPUCONFIG]
MPUSELECT = 0x000001FF
STARTADDR = 0x00000000
ENDADDR = 0xFFFFFFFF
MPPAVALUE = 0xFFFFFFFF
[MPUCONFIG]
MPUSELECT = 0x000002FF
STARTADDR = 0x00000000
ENDADDR = 0xFFFFFFFF
MPPAVALUE = 0xFFFFFFFF
[AIS_Set]
; Generic AIS set instruction to a reserved register to force a signature check
TYPE=2
ADDRESS=0x01E2C020
DATA=0
SLEEP=0