This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168 STOP AT STARTING KERNAL.....



Hello, I made 60 boards of 8168, 13 of them stop at the START KERNAL...... ,can not boot, the current does not fall detection, found that some can boot in a minute, and some can not, DDR adn NAND FLASH  testing in the CCS are no problems, I use the C version of the chip,i change 1 new 8168 chip in a board which having problem,then it is ok,i want to know WHAT IS THE PROBLEM,?THANKS