This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x, uboot cannot ping the board itself when set the phy into loopback mode?

Hi, All:

         I  am doing a phy lookpback test  with am335x, but it cannot work .  under normal mode ,the board can ping PC successfully.   when i set the phy into  loopback mode,   try to ping the board itself ,  and   found that  the cpsw‘driver cannot get the arp packet back.   However  i  probe rx pins between am335x and the phy, and fount that it   have the signal  when  sending  ping command. The board is beaglebone-black, and  the test  is  under uboot, (u-boot-2013.01.01-psp06.00.00.00) .

       Does anyone konw something about it?  thx in advance.