This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reading BAR data using C6678 as PCIe Root Complex with FPGA End Point



I am attempting to read data using a C6678 EVM from an FPGA dev board using PCIe. The C6678 is the RC and the FPGA is the EP on the PCIe bus.

The FPGA has the following BARs configured:

BAR0 - 0x0 - 0x3FFF (16 kB)
BAR1 - 0x0 - 0xFFFF (64 kB)
BAR2 - 0x0 - 0xFFFF (64 kB)
BAR3 - 0x0 - 0xFFFF (64 kB)
BAR4 - 0x0 - 0x1FFFF (128 kB)

The C6678 EVN (and PCIe carrier card) are connected to the FPGA board using a simple PCIe backplane that wires the PCIe connectors together. I previously verified the operation of the C6678 and FPGA cards by plugging them both into a Linux based PC. In this case, the Linux PC is acting as the RC on the PCIe bus for both devices and I am able to read and write to all of the BARs on both cards with no issues.

With the C6678 as the RC, I am able to perform link training and read the configuration registers on the FPGA. I can see the vendor ID and device number that match what was configured in the FPGA.

The problem I am having is reading the data from the FPGA. I am following the example in the PCIE_exampleProject and also some modifications that I found on the TI E2E forum. I modified the value of PCIE_IB_LO_ADDR_M and PCIE_OB_LO_ADDR_M to 0x0 to reflect the start address of the PCIe BAR. I also set PCIE_BAR_IDX_S and PCIE_BAR_IDX_M to 1. PcieModeGbl is also set to pcie_RC_MODE. 

The code in pcie_sample.c reports that it is successfully able to configure inbound and outbound translation. However when I try to read the BAR data using *((volatile uint32_t *)pcieBase + i) the data alternates between 0x60000000 and an sequence starting with 0x01 that increases in steps of 2.

Is the sequence I am seeing the default for the PCIe device memory upon initialization? 

Is there something else I need to set up to trigger a read from the FPGA (such as some sort of read request TLP)?

Are there any other settings that may need to be modified other than the values of PCIE_IB_LO_ADDR_M, PCIE_OB_LO_ADDR_M, PCIE_BAR_IDX_M and PCIE_BAR_IDX_S? 

Also does TI have an example code available beyond the pcie_sample.c file? The sample provided communicates only between two identical EVM cards and assumes the EP is pushing data back to the RC. I would like to find an example where the RC is initiating the data reads from an EP device.

Thanks,
-Bruce

  • Hi Bruce,

    TI doesn’t provide PCIE RC enumeration example/driver source. Normally the RC runs some operating system that performs the enumeration.

    In the MCSDK PCIe sample example, two DSP EVMs are used to test the PCIe driver. DSP 1 is configured as a Root Complex and DSP 2 is configured as End Point. Once the PCIe link is established, the following sequence of actions will happen:

    1. DSP 1 sends data to DSP 2 - DSP 2 waits to receive all the data

    2. DSP 2 sends the data back to DSP 1

    3. DSP 1 waits to receive all the data

    4. DSP 1 verifies if the received data matches the sent data and declares test pass or fail.

    Modified the value of PCIE_IB_LO_ADDR_M and PCIE_OB_LO_ADDR_M to PCIe inbound/outbound address. The BAR0 register is fixed to be mapped to PCIe application registers region. So the BAR0 mask setup does not affect BAR0 register. If you want to use 4 configurable BAR registers, please configure BAR1~BAR4 accordingly.

    Thanks,

  • Ganapathi,

    Can you provide some more information on the parameters needed for pcieBarCfg_t to map to the BARs I described above? I do not need to explicitly enumerate the BARs since these addresses will be fixed.

    To keep it simple, let's take BAR2 as an example. If I use the following code, I am able to successfully configure the BAR, but then the program stops working after that point:

    pcieBarCfg_t     barCfg;
    
    barCfg.location = pcie_LOCATION_REMOTE;
    barCfg.mode     = pcie_RC_MODE;
    barCfg.base     = 0x00000000;
    barCfg.prefetch = pcie_BAR_NON_PREF;
    barCfg.type     = pcie_BAR_TYPE32;
    barCfg.memSpace = pcie_BAR_MEM_IO;
    barCfg.idx      = 2;
    
    if ((retVal = Pcie_cfgBar(handle, &barCfg[i])) != pcie_RET_OK)
    {
       System_printf ("Failed to configure BAR%d (%d)\n", i, (int)retVal);
       exit(1);
    }
    else
    {
       System_printf("Configured BAR%d successfully!\n", i);
    }


    I also do not understand how to configure outbound translation when the BAR mappings in the FPGA all start with address 0x0. Is there a way to specify to the function pcieObTransCfg which BAR the mapping corresponds to?

    Thanks,
    -Bruce

  • Hi Bruce,

    PCIe BAR configuration details are clearly explained in PCIe user guide. Please take took at section 2.7.3 Use of Base Address Registers (BARs) on PCIe user guide.

    Also refer PCIe BAR configuration defined in IBL source code.

    Function: iblPCIeWorkaround()

    Path: “\ti\mcsdk_x_xx_xx_xx\tools\boot_loader\ibl\src\device\c66x\c66xinit.c”

    Thanks,

  • Ganapathi,

    I've looked at the PCIe user guide and c66xinit.c source code carefully, but the documentation is not clear on what steps are needed to enumerate and read data from a remote BAR when the C6678 is acting as the RC. If TI doesn’t provide PCIE RC enumeration example/driver source then I need to know who to contact to in order to get in this information.

    Here are the steps I am taking and maybe you can tell me what I am missing:

    -C6678 DSP eval board and FPGA eval board are connected via a PCIe backplane card.
    -Operation of each board in EP mode has been confirmed using a Linux PC.
    -C6678 has been set in RC mode, FPGA eval board in EP mode.


    -Set the OB_SIZE register to 0x3 and enable outboard address translation in the CMD_STATUS register.

    -Set the BAR addresses for BAR0 through BAR4 described described in my first post in the FPGA registers by specifying the pcie_LOCATION_REMOTE option. I assigned these addresses to the BARs: 

    0x00000000 to BAR0, 
    0x00100000 to BAR1, 
    0x00200000 to BAR2, 
    0x00300000 to BAR3, 
    0x00400000 to BAR4

    -Read the BAR addresses back out from the FPGA board and verified that they were set correctly.
    -Read the vendor ID and device ID from the FPGA board and verified that they are correct.

    -Configured outbound offsets in the pcie_LOCATION_LOCAL registers:

    Region 1: LO: 0x01, HI: 0x0
    Region 2: LO: 0x00100001, HI: 0x0
    Region 3: LO: 0x00200001, HI: 0x0
    Region 4: LO: 0x00300001, HI: 0x0
    Region 5: LO: 0x00400001, HI: 0x0

    -Perform a memcpy from the outbound address regions into a local buffer and print out the buffer. For example if I have a 1024 byte buffer declared as char buff[1024] and I want to read from BAR0 (which is mapped to region 1/address 0x60800000):

    memcpy(buff, 0x60800000, 1024);

    When I read the memory out of the buffer (or directly from the PCIESS address space), I just get garbage data.

    I've also tried to use an EDMA transfer, but that was not successful. I will probably try to use EDMA to optimize the transfer speed at some point, but for now, I just want to verify that I am able to transfer the correct data into memory using memcpy.

    -Bruce

     

  • Hi Bruce,

    The BAR0 register is fixed to be mapped to PCIe application registers region. So the BAR0 mask setup does not affect BAR0 register. If you want to use 4 configurable BAR registers, please configure BAR1~BAR4 accordingly. 

    Please go through below wiki for more information.

    http://processors.wiki.ti.com/index.php/PCI_Express_(PCIe)_Resource_Wiki_for_Keystone_Devices

    Thanks,

  • Ganapathi,

    Sorry for the delay in getting back to you. I've been reconfiguring the code I have to experiment with some different register settings.

    I've managed to be able to read data from BAR0 on the remote device, but I still cannot read from BAR1-BAR4. I've been through all of the documentation that TI has provided, but it's still not clear in describing how to configure the C6678 as RC. I see there have been several other posts on this E2E forum with similar questions but they do not seem to conclude with clear resolutions.

    It's my understanding that BAR0 is mapped to the PCIe application registers on the local device, but this restriction does not apply to outbound reads to an external device. The data I am reading from BAR0 on the remote device is not application register data.

    Can you take a look at the steps I outlined in my October 3rd post and clarify what I am missing or doing wrong?

    Thanks,

    -Bruce

  • Ganapathi,

    I've made some progress in reading the other BARs. It appears that the outbound address translation needs to be configured before the remote BAR addresses in order to work properly. 

    -Bruce

  • Hi Bruce,

    Thanks for your update.

    TI doesn’t provide PCIE RC enumeration example/driver source. Normally the RC runs some operating system that performs the enumeration with the following steps.

    If C66x device is configured as RC, then CFG_SETUP register is used to specify the target bus/device/function numbers for the target device (switch/EP) and try to read/write the remote device space in MMR (from offset 0x2000 in PCIe MMR space) to generate those configuration requests.

    Thanks,

  • Bruce,

    Here is what you need to do for performing a outbound read intiated by PCIE RC (TI DSP), read from PCIE EP (FPGA):

    - PCIE Link is up, I am sure you have this already

    - On RC side, configure OB_SIZE (0x2180_0030 to 3, which means 8MB each OB region, it is OK)

    - On RC side, configure CMD_STATUS (0x2180_0004), bit 1 to 1 for OB_XLT_EN

    - On RC side, you can use any OB regions, e.g 0x6000_0000, 0x6080_0000, 0x6100_0000 .... each 8MB size

    - Assuming you decided to use OB region 0x6080_0000, this is region 1, to read 1024 byte from FPGA

    - On RC  side, you need to program 0x2180_0208 and 0x2180_020c (they are OB_OFFSET_INDEX and OB_OFFSET_HI for OB region 1). The 0x2180_0208 needs to match one of the BAR in  the EP side, I don't know if you can use BAR0 or not on FPGA. Probalby you can only use BAR1, 2, 3, 4. So, you need to program 0x2180_0208 to 0x10_0001 if you intended to access BAR1, or, to 0x20_0001 for BAR2 ....,  For simplicity in the discussion, assume you wnat to access BAR 1, so you program it to 0x10_0001. For 0X2180_020C, it should be 0 since this is 32-bit BAR.

    What happens with this on RC side: when you read 0x6080_0000, it generates an outbound read to address 0x10_0000 across PCIE bus to EP side. 

    Then, on EP side, how they interpret this read, it first goes through BAR matching, then inbound translation. For your read from 0x10_0000, 0x10_0004, 0x10_0008 .... . It matches the BAR1 so accepted. Not sure if you have any inbound translation rule on EP side, if no, this will directly read above memory address on FPGA side. If yes, this read goes to some other FPGA memory location according to inbound translation. Hope this help!

    Regards, Eric

  • Thanks Eric! I managed to get outbound reads working for all of the BARs. As I mentioned in my reply to Ganapathi, it appears that outbound translation regions need to be configured before the remote BAR addresses are set. I'm not sure if that is particular to the FPGA card I am using as an EP or if that is something that applies to the PCIESS.

    The only other issue I'm having is that Region 0 behaves a little strangely. It reads some of the data, but sections that should be all zero are filled with 0xDEADBEEF. The problem went away when I moved the translation to Region 1. I don't need to use all of the regions that are available, so this is not really a problem for me. I just wanted to note it here in case someone is having a similar issue in the future.

    -Bruce

  • Bruce,

    Good to know the outbound read worked! "that outbound translation regions need to be configured before the remote BAR addresses are set", I don't see this is required. I often configure or reconfigure OB registers after remote BAR is set, my test setup is between TI PCIE device, not sure if anything particular for this FPGA. 

    My think is that, you don't need to program 0x2180_0208 and 0x2180_020c, just load the DSP RC code and run, before executing outbound read, you can set a break point there, so halt DSP and use CCS memory window to change those two registers then run, you should be able to read back the correct results. If you are interested, you can try. You can alos try to program those two to different BAR via CCS memory window, then you should read back different results.

    For BAR0, on our DSP, it is used to access remote side's PCIE application registers. For FPGA, I don't know if BAR0 is special as well, you may find it on data manual. Since you can use other BARs than BAR0, good to know it is OK for you.

    Regards, Eric   

  • Hello all,

    Bruce, i am having similar issues as your starting point...reading dev id, and link up but cant read data from Spartan6 FPGA...is it possible to share your eorking code please

  • How important is the choice of the Type0 or Type1 for RC and EP?

    As far as I understand this choice depends on the CFG_SETUP.CFG_TYPE setting.

    The SPRUGS6D says :

    Typically, a RC module uses Type 1 and EP configuration uses Type 0 configuration space.

    But in example 

    C:\ti\pdk_C6670_1_1_2_6\packages\ti\drv\pcie\example\sample\pcie_sample.c

    CFG_TYPE bit of CFG_SETUP registr is set to "0" for RC and for EP. And so RC configured as Type 0 and EP too.

    Why?  Is it importently or no?

    Should CFG_SETUP.CFG_TYPE be changed  fo RC on"1" (Type1)?

     

    With regards, Alexander.

  • Hi,

    In the MCSDK PCIe sample example,  DSP 1 is configured as a Root Complex and DSP 2 is configured as End Point by own test application. For  test the PCIe driver between two DSP devices.

    Thanks,

  • Hi Bruce,

    I am also experimenting on the PCie, I had following question,

    From driver point of view, the Endpoint will have same BAR address for data read/write.

    For example purpose, let us assume that we have configured address 0x8A000000 as BAR address in configuration space of EP at logical address Bus_id=0, dev_id=0 and fun_id=0.

    For Linux OS, when driver requests memory resource for EP 0, the address 0x8A000000 will be returned by the PCIe stack. Now for any read/write for the end-point will through 0x8A000000 from driver.

    But PCIe requires the BAR address to be different for outbound transfer(For data write and read request packets) and inbound transfer for inbound packets.

    So how is that the same BAR address is maintained for read and write in driver

    Thanks in advance