Other Parts Discussed in Thread: OMAPL138
hi, i'm building a simple simulink model, the input is const 1(frame based),output is C6748 EVM from embeded coder block. I want to generate .out file from matlab to ccsv5. however there are errors:
"### Creating standalone executable "../untitled.exe" ..."
C:/PROGRA~1/MATLAB/R2014a/sys/lcc64/lcc64/bin/lcclnk64 -s -LC:/PROGRA~1/MATLAB/R2014a/sys/lcc64/lcc64/lib64 -o ../untitled.exe @untitled.lnk rt_main.obj
untitled.obj .text: undefined reference to 'dacXmt'
untitled.obj .text: undefined reference to 'dacCodecInit'
gmake: *** [../untitled.exe] Error 2
~\Documents\MATLAB\untitled_grt_rtw>echo The make command returned an error of 2
The make command returned an error of 2
~\MATLAB\untitled_grt_rtw>An_error_occurred_during_the_call_to_make
'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command,
operable program or batch file.
does anyone know how to modify this? thanks in advance!