This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Symmetric fir function in CSL 3.00 for TI C5505



I'm using the firs.asm function in the CSL3.00.00 library for the C5505 DSP. I have a symmetric filter with even number of taps. I feed both the x and h vectors into the function, and specify nh = length(h)/2, to account for symmetry.

I see it works fine for even number of taps, but how do I indicate to the function that I have symmetric filter with odd number of taps?

Chris