Other Parts Discussed in Thread: CC3100, CC3200, CC3100SDK, TM4C1294NCPDT, MSP430F5529, CC31XXEMUBOOST
Hello,
I have been trying to get the iPhone CC3100 SimpleLink application to work for a couple of days with no luck. I downloaded from the Apple App Store the SimpleLink WiFi Starter. I installed it on my phone with no issues. I did check the App site and it indicated that it was for the CC3100. My problem is that it does not connect to the CC3100 in station mode. I put in the SSID and password and press start but the application just sites their until it times out. I have been successfully able to set up the CC3100 by using it in AP mode without the iPhone application. I put the CC3100 in AP mode and then us my PC to connect to the AP website, http://simplelink.net, and set the CC3100 station SimpleLink parameters in the setup page. When I do this the tcpEchoCC3100_TM4C1249NCPDT works fine. When I try to use the iPhone application I get nothing. The release version of the iPhone SimpleLink WiFi Starter application is 1.0. Is anyone else having the same problems?
Best Regards,
Steve Mansfield