Hi,
In my design I am using the TMS320C6672ACYP DSP and I am sharing the SPI-wires with an external flash and another device.
The problem that I have with this, is that if I would like to program the flash (quad SPI device) during boundary scan, I get contention on my SPI-wires D0 and D1, which are connected to my flash device as well as another device.
This problem could be resolved if I had a BSDL file in which it would be possible to drive the TMS320C6672ACYP in High-Z mode during boundary scan. Is there a BSDL model for this device that is capable of doing this?
Please advise.
Regards,
Danny