Hi All,
I have a question regarding TI Desktop Linux SDK and Advantech DSPC-8681 card. My configuration is as follows:
Server: HP-DL380
OS: Red Hat Enterprise Linux Server release 6.2 (Santiago)
Advantech DSPC-8681 PCIE card (A103 HW Revision)
Testing with new TI Desktop Linux SDK driver (latest maintenance release version 01.00.02.00 Build date: 03132014).
Built the new driver and performed the following tests loading driver and reset dsps.
The NMI message is seen after dspallreset.sh command is issued “kernel:NMI: IOCK error (debug interrupt?)”, however no error is seen on the iLO Event Log.
Anyone have any experience with this type of error message or are there any patches to the driver code that can resolve it?
Thanks,
James
[root@0-9 memtest]# ./driver_init.sh
Executing dummy application to set permissions for pci memory windows
drv api open complete
Contiguous memory alloc complete
mem range alloc complete
Map dsp mem range complete
DSP Init global shared complete !
[root@0-9 memtest]# ./dspallreset.sh
Message from syslogd@0-9 at Oct 3 01:45:00 ...
kernel:NMI: IOCK error (debug interrupt?)
Num of devices 4
Message from syslogd@0-9 at Oct 3 01:45:00 ...
kernel:Stack:
Message from syslogd@0-9 at Oct 3 01:45:00 ...
kernel:Call Trace:
Message from syslogd@0-9 at Oct 3 01:45:00 ...
kernel:Code: 8b 34 25 c8 cb 00 00 48 89 d1 48 8d 86 38 e0 ff ff 0f 01 c8 0f ae f0 48 8b 86 38 e0 ff ff a8 08 75 09 48 89 d8 4c 89 e1 0f 01 c9 <48> 8b 5d d8 4c 8b 65 e0 4c 8b 6d e8 4c 8b 75 f0 4c 8b 7d f8 c9
Iterations waited for entry point to clear 1
Dsp 0: DSP Reset success !
Iterations waited for entry point to clear 1
Dsp 1: DSP Reset success !
Iterations waited for entry point to clear 1
Dsp 2: DSP Reset success !
Iterations waited for entry point to clear 1
Dsp 3: DSP Reset success !