Other Parts Discussed in Thread: UCD74120, UCD9224
Hello
We are developing a data acquisition board using 66AK2HAAAW24 DSPs. As described in the K2 datasheet, there is only one SmartReflex (SR) interface on the following pins: AT39, AR37, AR36, AT38, AU38, AR35.
In the schematics drawings of the evaluation board "K2H_K2EVM-HK_SCH_A104_REV3_0.DSN" there are two SR interfaces, one for DSP and another one for ARM where it is defined at reserved pins: AU36, AV37, AU37, AV36, AU35, AW36.
There is no any information on the SR interface for the ARM in the documentation of the K2.
The question is if we can use the a fixed power for the ARM core, as defined in the HW design guide, or we need implement the SR circuit?
Regards
Moshe Lerner