Other Parts Discussed in Thread: TVP7002
Hello,
On DM365 I need to capture BT656 with embedded syncs from an external video module that provides video in this format. It seems to me that current drivers are "tied" to one of the supported video decoders (i.e. TVP7002, TVP514x, etc). In my case there is no decoder at all, so I'd like to use existing vpfe software support to capture BT656 without having to load any specific decoder driver. Is there any "vanilla capture" driver I can use or must I rewrite a "fake decoder" driver?