Other Parts Discussed in Thread: TMS320C5515
Hi, I use CCS 6.0 and TMS320C5515 eZDSP USB Stick Development Tool. I try an example
csl_usb_cdc_example from CSL library. It works, I can receive and transmit data but
suspending is not working - I get message "USB Suspend failed". Which is quite interesting,
the message "CSL CDC Module Open Successful" is printed twice.
My problem is that if I start debugging and then stop debugging and then launch the program
again, I get the following error:
"Error connecting to the target:
(Error -1138 @ 0x5F)
Device refused to allow debug mode. Power-cycle the board. If error persists, confirm
configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.507.0)".
After re-plugging both USB cables (one for debugging and one for communication), everything is OK, but it's quite inconvenient to re-plug device before each program launch. Any advices?
Best regards,
Natalia.