Other Parts Discussed in Thread: OMAPL138, TMS320C6748
What could be the best choice for a simple DSP application?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAPL138, TMS320C6748
What could be the best choice for a simple DSP application?
Please do not duplicate your posts...you posted same question here http://e2e.ti.com/support/dsp/c5000/f/109/t/373593.aspx
Our apps team will be replying to you....
Hi,
Thanks for your post.
In my opinion, C6748 processor would be the right choice for low power and low cost solutions for audio based applications. There is a C6748/OMAPL138 LCDK development tool which is easy-to-use, affordable and scalable.
L138/C6748 development kit is part of single core DSP kit includes either a TMS320C6748 DSP or an OMAPL138 application processor with 456 MHz C674x Fixed/Floating point core. It has On-chip RTC, DDR2 running at 150 MHz, NAND FLASH and SD/MMC Slot, USB Serial Port, Fast Ethernet Port, B Host port (USB 1.1), USB OTG port (USB 2.0), SATA Port , VGA port, LCD Port (Beagleboard XM connectors), three AUDIO Ports, Composite IN (RCA Jack) and Leopard Imaging Camera Sensor Input.
For more details on C6748/OMAPL138 LCDK, please refer the below wiki:
http://processors.wiki.ti.com/index.php/L138/C6748_Development_Kit_(LCDK)
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------
Hi,
Thanks for your update.
If this is the case, please download the TI C67x DSPLIB from the below link in which you could see filtering and convolution libaray functions:
http://www.ti.com/tool/sprc121
For C674x device, please check the supported kernel functions for C674x DSP_LIB from the below wiki:
http://processors.wiki.ti.com/index.php/C674x_DSPLIB#DSPF_sp_fir_gen_.28FIR_Filter.29
Also, please refer the c67x DSP FIR/IIR signal processing examples from the application report as given below:
http://www.ti.com/lit/an/spra947a/spra947a.pdf
Kindly check the c67x DSP library programmer's guide for filtering and convolution functions as below:
http://www.ti.com/lit/ug/spru657c/spru657c.pdf
The sample example code with the project from DSPF_sp_fir_gen can be found in the DSPLIB package under the path ~\ti\dsplib_c674x_3_2_0_1\packages\ti\dsplib\src\DSPF_sp_fir_gen. Please give it a try to see the sample implementation and check to see , how the API's are used for the same.
Thanks & regards,
Sivaraj K