This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTC_VSS on C6748

Hey,


On the TMS320C6748BZWTA3, pin H18 is RTC_VSS.  In the development board, this pin is also connected to the crystal capacitors for the RTC crystal.  However, this signal is not connected anywhere else.  Is this correct?  There is a battery that powers RTC_CVDD (L14), but this is connected to CVI_AGND, not RTC_VSS.

Should RTC_VSS be connected to anything or should it be left floating?

Thanks,

Tobyn