Other Parts Discussed in Thread: SYSBIOS
Good day to all,
I have created a MessageQ project from the IPC MessageQ Single Image example project. In the project, the messageQ bounce messages between cores and uses System_printf to output the messages. Is it possible for me to use platform_write instead? But platform_write uses printf, so i just #include <stdio.h> in my messageQ project will do? I wanted to try using platform_write and burn the program into my DSP EVM6678LE, so that i can check for the output via serial.
When i added platform_write and compile, i receive the error stating that the program cannot fit into the memory. So i went to other sys/bios projects and copied sections of codes from the .cfg file over to the MessageQ's .cfg file. Code copied are shown below:
var heapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var heapMemParams = new HeapMemParams();
heapMemParams.size = 0x200000;
heapMemParams.SectionName = "systemHeap";
Program.global.heap0 = HeapMem.create(heapMemParams);
Program.sectMap["sharedL2"] = "DDR3";
....
....
<all the various sectMaps here, my workstation isnt connected to the internet so i couldn't copy and paste>
....
....
Program.sectMap["far:NDK_PACKETMEM"] = {loadSegment: "L2SRAM", loadAlign: 128};
After adding the above codes, the error regarding unable to fit program to memory is gone. But when i tried doing a few printf etc the following error appears: (as i could not copy and paste the exact error message from my offline workstation, the following code is copied online, just to give a rough idea what kind of error message i'm seeing)
- [C66xx_2] A0=0x0 A1=0x0
- [C66xx_2] A2=0x0 A3=0x0
- [C66xx_2] A4=0x0 A5=0x1
- [C66xx_2] A6=0x193 A7=0x0
- [C66xx_2] A8=0xc0006ec A9=0x1
- [C66xx_2] A10=0xfffffffc A11=0x2
- [C66xx_2] A12=0x0 A13=0xc0000b8
- [C66xx_2] A14=0xc0006ec A15=0xc195830
- [C66xx_2] A16=0xc205780 A17=0x10
- [C66xx_2] A18=0x806780 A19=0x30
- [C66xx_2] A20=0x6c A21=0x4c
- [C66xx_2] A22=0x40100581 A23=0xb040
- [C66xx_2] A24=0x420880 A25=0x8031000c
- [C66xx_2] A26=0x84605 A27=0x60800006
- [C66xx_2] A28=0x20000 A29=0x0
- [C66xx_2] A30=0xc1932dc A31=0x0
- [C66xx_2] B0=0x1 B1=0x0
- [C66xx_2] B2=0x0 B3=0xc323e24
- [C66xx_2] B4=0x2 B5=0xc1930a8
- [C66xx_2] B6=0xf580010 B7=0xc192af0
- [C66xx_2] B8=0x0 B9=0x0
- [C66xx_2] B10=0x90 B11=0x1
- [C66xx_2] B12=0x2 B13=0xc37b1e0
- [C66xx_2] B14=0x806f98 B15=0x8068c8
- [C66xx_2] B16=0x8068b8 B17=0x0
- [C66xx_2] B18=0xc0004f0 B19=0xc
- [C66xx_2] B20=0x69 B21=0x3
- [C66xx_2] B22=0x3 B23=0x0
- [C66xx_2] B24=0x9c002cc4 B25=0xc4002200
- [C66xx_2] B26=0x304482 B27=0x22400302
- [C66xx_2] B28=0x420a0900 B29=0x8005202a
- [C66xx_2] B30=0x0 B31=0x1
- [C66xx_2] NTSR=0x1000c
- [C66xx_2] ITSR=0x0
- [C66xx_2] IRP=0x0
- [C66xx_2] SSR=0x0
- [C66xx_2] AMR=0x0
- [C66xx_2] RILC=0x0
- [C66xx_2] ILC=0x0
- [C66xx_2] Exception at 0x0
- [C66xx_2] EFR=0x2 NRP=0x0
- [C66xx_2] Internal exception: IERR=0x1
- [C66xx_2] Instruction fetch exception
- [C66xx_2] ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x00000000, sp = 0x008068c8.
- [C66xx_2] xdc.runtime.Error.raise: terminating execution
Am i doing things wrongly? If so how do i rectify them?