Hello,
the demo-program "Blink an on-board LED" only works under the following surface:
but not, when I run it under Cloud9:
I can even make syntax errors. There is no complain for the non-working code and (still) the LED is not blinking:
Am I missing a setting that I would have to make?
Should I update debian?
Beaglebone black: Element14, rev. C
Windows: XP
Best regards,