Other Parts Discussed in Thread: SYSBIOS
Hi
I am developing for a Keystone2 device using CCS 5.5 and CGT 7.4.4. When the build system compiles the .cfg file I get errors indicating mismatch of compiler version (please see below). Does this mean that I am using the wrong core libraries?
'Invoking: XDCtools'
"/ti/xdctools_3_25_02_70/xs" --xdcpath="/ti/pdk_keystone2_3_00_03_15/packages;/ti/bios_6_35_04_50/packages;/ti/syslib_3_00_01_00/packages;/ti/salld_keystone2_02_00_02_00/packages;/ti/ipc_3_00_04_29/pa
ckages;/ti/xdais_7_21_01_07/packages;/ti/uia_1_03_00_02/packages;/ti/sc_lte_sdk_04_01_lwp1410_premium/snow3g_1_0_0_1/packages;/ti/sc_lte_sdk_04_01_lwp1410_premium/sa3gpp_keystone2_02_00_02_00/packages
" xdc.tools.configuro -o ./Debug/configPkg -t ti.targets.elf.C66 -p "ti.platforms.evmTCI6638K2K:LTE" -r debug -b "..\..\..\..\lteenodeb/l2/build/HAWKING/tmdxevm_lteL2Config.bld" -c "/ti/ccsv5/tools/co
mpiler/c6000_7.4.4" "..\..\..\..\lteenodeb/l2/build/lteL2Core3.cfg"
configuring lteL2Core3.xe66 from package/cfg/lteL2Core3_pe66.cfg ...
js: "C:/ti/xdctools_3_25_02_70/packages/xdc/cfg/Main.xs", line 160: Error: xdc.cfg.INCOMPATIBLE_TARGET_VERSION: the compiler version [] used by the current target 'ti.targets.elf.C66' is not compatibl
e with compiler version of targets used to build the following packages; package ti.targets.rts6000 [in C:/ti/xdctools_3_25_02_70/packages/ti/targets/rts6000/] was built using the target 'ti.targets.e
lf.C66' with compiler version [7.2.0].
; package ti.sysbios.family.c64p [in C:/ti/bios_6_35_04_50/packages/ti/sysbios/family/c64p/] was built using the target 'ti.targets.elf.C66' with compiler version [7.2.0].
; package ti.sysbios.hal [in C:/ti/bios_6_35_04_50/packages/ti/sysbios/hal/] was built using the target 'ti.targets.elf.C66' with compiler version [7.2.0].
; package ti.sysbios.knl [in C:/ti/bios_6_35_04_50/packages/ti/sysbios/knl/] was built using the target 'ti.targets.elf.C66' with compiler version [7.2.0].
; package ti.sysbios.heaps [in C:/ti/bios_6_35_04_50/packages/ti/sysbios/heaps/] was built using the target 'ti.targets.elf.C66' with compiler version [7.2.0].