Hi All,
I Need to configure the 4GB micron eMMC device with AM335X MMC1 interface of TI SDK7.00 source .
1.eMMC integration in kernel level,what are all changes i want to make it as to working condition of eMMC.
2.eMMC API's call to check the eMMC read /write cycle and verifying the written data.
3.In SDK7 which one is the eMMC driver?
drivers/mmc/host/omap_hsmmc.c ----> This driver file is correct one or not.
4.eMMC partition and formatting commands
fdisk--> this is command correcrt for to fprmat the eMMC device.
Thanks by,
Venkat