1. I had hoped to get the c6x port of uclinux running in 32MB of memory using a minimal initramfs. But it would seem that 48M is needed for a successful boot. Less than this does not lead to a shell prompt:
Freeing unused kernel memory: 140K freed
/init: '/lib/libc.so.0' is not an ELF file
/init: '/lib/libc.so.0' is not an ELF file
/initlibc.so.0Kernel panic - not syncing: Attempted to kill init!
2. the real requirement is to run racoon as an IKE daemon. I can't get this to run in less than 64MB of memory. Any less than this and starting racoon (or openssl for that matter) produces failures to load libc
/ # racoon -v -ddd -F
racoon:597: can't map '/lib/libc.so.0'
racoon:597: can't map '/lib/libc.so.0'
racoon: can't load library 'libc.so.0'
I see that openWrt seem to manage to run libcrypto (openssl) based applications with less resources. Is there anything that I can do to improve my chances?
Thanks