This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x smartreflex driver for recent kernels

Hi!

I can't seem to get smartreflex working on a custom am335x based board with the 3.12 kernel from the latest SDK. It worked in the previous SDKs, which was based on kernel 3.2. Investigating it further it seems that am335x used a special smartreflex driver, called am335x_smartreflex.c which exists as a patch in the previous SDKs. But it seems to be missing in the latest SDK.
It says in a comment in the patch that work is being conducted in pushing the driver upstreams. But I see no signs of the driver in the ti kernel. Furthermore I found this somewhat cryptic message in the kernel release notes from the latest SDK, 07.00.00,

B-02423 AVS missing from integration tree

So what is TI's plan regarding smartreflex in am335x? Are you planning to maintain the driver and make it work on newer kernels or are you going to drop smartreflex support in am335x? Or am I missing something? AFAIK the smartreflex drivers already in the kernel tree doesnt work on am335x.

Regards,

Mårten