Other Parts Discussed in Thread: OMAP3530
While looking through the block diagram in the OMAP3530 documentation, I noticed that both the RAM and ROM list both 'public' and 'secure' memory ('64K on-chip RAM 2KB public/ 62KB secure' and '112K on-chip ROM 80KB secure/ 32KB BOOT'). I can guess what the boot ROM might be, but I haven't had any luck finding the difference between 'public' and 'secure' memory, either in general, or in reference to the OMAP3530.
Could anyone enlighten me as to this difference, or provide a pointer to some resources that would help me with this?