Hello,
I finally got my AM335x custom board to successfully kexec.
I have one remaining problem after kexec:
Regular booting, soft/hard, gives the following line in dmesg:
Detected MACID = 1c:ba:8c:b6:c1:0d
However, when I kexec back into the same kernel, dmesg gives:
Random MACID = 6a:60:fb:40:16:40
Can someone help with this?
When does the cpsw driver get initialized with the correct MAC ID?
Thanks
Brian