This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP34x-II Zoom Mobile Development board : FAULTY BOARD

Hi,
 We are having a faulty board here,we observed that graphics comes up
 on the board and on hooking up with serial , console is hung , lv8093
 2-0072: Registered lv8093 as V4L2 device.
 mmc1: new MMC card at address 0001
 Registered lv8093 as i2c device.
 mmcblk1: mmc1:0001 SDM032 30.6 MiB
mmcblk1:<6>twl4030_rtc twl4030_rtc: setting system clock to 2000-01-01
 00:01:20 UTC (946684880) ma``i!0 `adpqihe aqahe aahede ``maa
 `aa`Mhoib, .
 
Please suggest.
Regards,
Umang Gupta

  •  

    CONSOLE LOGS  For Above issue :

     

    > U-Boot 1.1.4-dirty (Mar 27 2009 - 11:27:11)
    >
    > OMAP3430-GP rev 2, CPU-OPP2 L3-165MHz
    > OMAP3430LAB 0.1 Version + mDDR (Boot NAND)
    > DRAM: 256 MB
    > NAND:512 MiB
    >
    > Reading data from 0xdf800 -- 100% complete.
    > In: serial
    > Out: serial
    > Err: serial
    > Hit any key to stop autoboot: 0
    >
    > 2792352 bytes read
    > ## Booting image at 80000000 ...
    > Image Name: Linux-2.6.29.6-omap1
    > Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2792288 Bytes = 2.7 MB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK OK
    >
    > Starting kernel ...
    >
    > Uncompressing
    > Linux.............................................................................................
    > Linux version 2.6.29.6-omap1 (root@deepak) (gcc version 4.3.2 (Sourcery
    > G++ Lite 2008q3-72) ) #16 PREEMPT Thu J0
    > CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c5387f
    > CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
    > Machine: OMAP ZOOM2 board
    > Memory policy: ECC disabled, Data cache writeback OMAP3430 ES3.1
    > SRAM: Mapped pa 0x40200000 to va 0xe3000000 size: 0x100000 Reserving 4194304 bytes SDRAM for VRAM Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 Kernel command line: console=ttyS3,115200n8 root=/dev/mmcblk0p2 rw ip=off mem=256M devfs=mount init=/init Clocking rate (Crystal/DPLL/ARM core): 26.0/166/500 MHz GPMC revision 5.0
    > IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts Total of 96 interrupts on 1 active controller OMAP34xx GPIO hardware version 2.5 PID hash table entries: 1024 (order: 10, 4096 bytes) OMAP clockevent source: GPTIMER1 at 32768 Hz
    > Console: colour dummy device 80x30
    > Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    > Memory: 256MB = 256MB total
    > Memory: 249344KB available (5260K code, 779K data, 180K init) Calibrating delay loop... 498.87 BogoMIPS (lpj=1945600) Mount-cache hash table entries: 512
    > CPU: Testing write buffer coherency: ok
    > net_namespace: 520 bytes
    > regulator: core version 0.5
    > NET: Registered protocol family 16
    > MUX: setup H18_34XX_GPIO163 (0xd800219a): 0x0108 -> 0x011c
    > MUX: setup B24_34XX_GPIO101_OUT (0xd800211a): 0x0104 -> 0x0004
    > MUX: setup A24_34XX_GPIO94 (0xd800210c): 0x0007 -> 0x0104
    > MUX: setup C25_34XX_GPIO96 (0xd8002110): 0x0000 -> 0x0004
    > MUX: setup H16_34XX_SDRC_CKE0 (0xd8002262): 0x0118 -> 0x0000
    > MUX: setup H17_34XX_SDRC_CKE1 (0xd8002264): 0x0118 -> 0x0000 OMAP DMA hardware revision 4.0
    > bio: create slab <bio-0> at 0
    > i2c_omap i2c_omap.1: bus 1 rev3.12 at 100 kHz
    > twl4030: PIH (irq 7) chaining IRQs 368..375
    > twl4030: power (irq 373) chaining IRQs 376..383
    > twl4030: gpio (irq 368) chaining IRQs 384..401
    > twl4030_mmc_init:362
    > twl4030_mmc_init:377
    > twl4030_mmc_init:377
    > twl4030_mmc_init:377
    > MUX: setup M27_3430_MMC1_CMD (0xd8002146): 0x0118 -> 0x0000
    > MUX: setup P27_3430_MMC1_DAT4 (0xd8002150): 0x0018 -> 0x0118
    > MUX: setup P26_3430_MMC1_DAT5 (0xd8002152): 0x0018 -> 0x0118
    > MUX: setup R27_3430_MMC1_DAT6 (0xd8002154): 0x0018 -> 0x0118
    > MUX: setup AE2_3430_MMC2_CLK (0xd8002158): 0x0101 -> 0x0100
    > MUX: setup AG5_3430_MMC2_CMD (0xd800215a): 0x0101 -> 0x0118
    > MUX: setup AH5_3430_MMC2_DAT0 (0xd800215c): 0x0101 -> 0x0118
    > MUX: setup AH4_3430_MMC2_DAT1 (0xd800215e): 0x011c -> 0x0118
    > MUX: setup AG4_3430_MMC2_DAT2 (0xd8002160): 0x0009 -> 0x0118
    > MUX: setup AF4_3430_MMC2_DAT3 (0xd8002162): 0x0109 -> 0x0118
    > MUX: setup AF10_3430_MMC3_CLK (0xd80025d8): 0x001b -> 0x011a
    > MUX: setup AC3_3430_MMC3_CMD (0xd80021d0): 0x000b -> 0x011b
    > MUX: setup AE11_3430_MMC3_DAT0 (0xd80025e4): 0x0103 -> 0x011a
    > MUX: setup AH9_3430_MMC3_DAT1 (0xd80025e6): 0x0103 -> 0x011a
    > MUX: setup AF13_3430_MMC3_DAT2 (0xd80025e8): 0x0103 -> 0x011a
    > MUX: setup AE13_3430_MMC3_DAT3 (0xd80025e2): 0x0103 -> 0x011a
    > regulator: VMMC1: 1850 <--> 3150 mV normal standby
    > regulator: VDAC: 1800 mV normal standby
    > regulator: VUSB1V5: 1500 <--> 0 mV normal standby
    > regulator: VUSB1V8: 1800 <--> 0 mV normal standby
    > regulator: VUSB3V1: 3100 <--> 0 mV normal standby
    > regulator: VMMC2: 1850 mV normal standby
    > regulator: VSIM: 1800 <--> 3000 mV normal standby i2c_omap i2c_omap.2: bus 2 rev3.12 at 100 kHz i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz SCSI subsystem initialized twl4030_usb twl4030_usb: Initialized TWL4030 USB module
    > usbcore: registered new interface driver usbfs
    > usbcore: registered new interface driver hub
    > usbcore: registered new device driver usb
    > Bluetooth: Core ver 2.15
    > NET: Registered protocol family 31
    > Bluetooth: HCI device and connection manager initialized
    > Bluetooth: HCI socket layer initialized
    > cfg80211: Using static regulatory domain info
    > cfg80211: Regulatory domain: US
    > (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp) (2402000 KHz - 2472000 KHz @ 40000 KHz), (600 mBi, 2700 mBm) (5170000 KHz - 5190000 KHz @ 40000 KHz), (600 mBi, 2300 mBm) (5190000 KHz - 5210000 KHz @ 40000 KHz), (600 mBi, 2300 mBm) (5210000 KHz - 5230000 KHz @ 40000 KHz), (600 mBi, 2300 mBm) (5230000 KHz - 5330000 KHz @ 40000 KHz), (600 mBi, 2300 mBm) (5735000 KHz - 5835000 KHz @ 40000 KHz), (600 mBi, 3000 mBm)
    > cfg80211: Calling CRDA for country: US
    > musb_hdrc: version 6.0, musb-dma, host, debug=0
    > musb_hdrc: USB Host mode controller at d80ab000 using DMA, IRQ 92 musb_hdrc musb_hdrc: MUSB HDRC host driver musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1 usb usb1: configuration #1 chosen from 1 choice hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected
    > NET: Registered protocol family 2
    > IP route cache hash table entries: 2048 (order: 1, 8192 bytes) TCP established hash table entries: 8192 (order: 4, 65536 bytes) TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
    > TCP: Hash tables configured (established 8192 bind 8192) TCP reno registered
    > NET: Registered protocol family 1
    > zoom2_wifi_init: start
    > omap-iommu omap-iommu.1: isp registered
    > NetWinder Floating Point Emulator V0.97 (double precision)
    > ashmem: initialized
    > VFS: Disk quotas dquot_6.5.2
    > Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    > JFFS2 version 2.2. (NAND)  © 2001-2006 Red Hat, Inc.
    > yaffs Jan 21 2010 12:08:16 Installing.
    > msgmni has been set to 487
    > alg: No test for stdrng (krng)
    > io scheduler noop registered
    > io scheduler anticipatory registered (default) io scheduler deadline registered io scheduler cfq registered OMAP DSS rev 2.0 OMAP DISPC rev 3.0 OMAP VENC rev 2
    > Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    > serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
    > serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
    > serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
    > serial8250.0: ttyS3 at MMIO 0x10000000 (irq = 262) is a ST16654 console [ttyS3] enabled
    > brd: module loaded
    > loop: module loaded
    > eth0 (smc911x): not using net_device_ops yet
    > eth0: LAN9221 (rev 0) at 0x8000000 IRQ 318
    > eth0: Ethernet addr: 00:00:00:00:82:a8
    > Broadcom 43xx driver loaded [ Features: , Firmware-ID: FW13 ] Broadcom 43xx-legacy driver loaded [ Features: ID, Firmware-ID: FW10 ]
    > usbcore: registered new interface driver rt73usb Linux video capture interface: v2.00 omap-previewer omap-previewer: omap-previewer: Registered preview wrapper omap-iommu omap-iommu.1: isp: version 1.1 i2c /dev entries driver Driver 'sd' needs updating - please use bus_type methods omap2-nand driver initializing NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron NAND 512MiB 1,8V 16-bit) Creating 7 MTD partitions on "omap2-nand.0":
    > 0x000000000000-0x000000080000 : "X-Loader-NAND"
    > 0x000000080000-0x000000100000 : "U-Boot-NAND"
    > 0x000000100000-0x000000140000 : "Boot Env-NAND"
    > 0x000000140000-0x000000540000 : "Kernel-NAND"
    > 0x000000540000-0x000010540000 : "system"
    > 0x000010540000-0x000014540000 : "userdata"
    > 0x000014540000-0x000018540000 : "cache"
    > Initializing USB Mass Storage driver...
    > usbcore: registered new interface driver usb-storage USB Mass Storage support registered.
    > udc: OMAP UDC driver, version: 4 October 2004 (iso) (dma) android init
    > mice: PS/2 mouse device common for all mice
    > input: TWL4030 Keypad as
    > /devices/platform/i2c_omap.1/i2c-adapter/i2c-1/1-004a/twl4030_keypad/input/input0
    > i2c_omap i2c_omap.2: Transmit error
    > synaptics_ts_probe: Product Major Version 1
    > synaptics_ts_probe: Product Minor Version 5
    > synaptics_ts_probe: product property 2
    > synaptics_ts_probe: device control 81
    > synaptics_ts_probe: interrupt enable 3
    > synaptics_ts_probe: 0xe0: 1 1 1 2 1 5 0 0
    > synaptics_ts_probe: Sensor properties 601
    > synaptics_ts_probe: max_x 7515, max_y 4667
    > synaptics_ts_probe: inactive_x 0 0, inactive_y 0 0
    > synaptics_ts_probe: snap_x 0-0 0-0, snap_y 0-0 0-0
    > input: synaptics-rmi-touchscreen as /devices/virtual/input/input1
    > synaptics_ts_probe: Start touchscreen synaptics-rmi-touchscreen in interrupt mode twl4030_rtc twl4030_rtc: rtc core: registered twl4030_rtc as rtc0 Driver for 1-wire Dallas network protocol.
    > omap_hdq omap_hdq.0: OMAP HDQ Hardware Rev 0.5. Driver in Interrupt mode w1_master_driver w1 bus master: Family 1 for 01.000000000000.3d is not registered.
    > Android battery driver installed
    > OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
    > Bluetooth: Virtual HCI driver ver 1.2
    > Bluetooth: HCI UART driver ver 2.2
    > Bluetooth: HCI H4 protocol initialized
    > Bluetooth: HCI BCSP protocol initialized
    > Bluetooth: HCILL protocol initialized
    > Bluetooth: Broadcom Blutonium firmware driver ver 1.2
    > usbcore: registered new interface driver bcm203x
    > Bluetooth: Digianswer Bluetooth USB driver ver 0.10
    > usbcore: registered new interface driver bpa10x
    > Bluetooth: BlueFRITZ! USB driver ver 1.2
    > usbcore: registered new interface driver bfusb
    > Bluetooth: Generic Bluetooth USB driver ver 0.5
    > usbcore: registered new interface driver btusb
    > Bluetooth: Generic Bluetooth SDIO driver ver 0.1
    > cpuidle: using governor ladder
    > cpuidle: using governor menu
    > regulator: Unable to get requested regulator: vmmc_aux
    > regulator: Unable to get requested regulator: vmmc
    > usbcore: registered new interface driver usbhid
    > usbhid: v2.6:USB HID core driver
    > logger: created 64K log 'log_main'
    > logger: created 256K log 'log_events'
    > logger: created 64K log 'log_radio'
    > Advanced Linux Sound Architecture Driver Version 1.0.18a.
    > No device for DAI twl4030
    > No device for DAI twl4030 Voice
    > No device for DAI omap-mcbsp-dai-0
    > No device for DAI omap-mcbsp-dai-1
    > No device for DAI omap-mcbsp-dai-2
    > No device for DAI omap-mcbsp-dai-3
    > No device for DAI omap-mcbsp-dai-4
    > Zoom2 SoC init
    > TWL4030 Audio Codec init
    > asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
    > asoc: twl4030 Voice <-> omap-mcbsp-dai-1 mapping ok ALSA device list:
    > #0: Zoom2 (twl4030)
    > TCP cubic registered
    > Initializing XFRM netlink socket
    > NET: Registered protocol family 17
    > NET: Registered protocol family 15
    > Bluetooth: L2CAP ver 2.13
    > Bluetooth: L2CAP socket layer initialized
    > Bluetooth: SCO (Voice Link) ver 0.6
    > Bluetooth: SCO socket layer initialized
    > Bluetooth: RFCOMM socket layer initialized
    > Bluetooth: RFCOMM TTY layer initialized
    > Bluetooth: RFCOMM ver 1.11
    > Bluetooth: BNEP (Ethernet Emulation) ver 1.3
    > Bluetooth: BNEP filters: protocol multicast
    > Bluetooth: HIDP (Human Interface Emulation) ver 1.2
    > RPC: Registered udp transport module.
    > RPC: Registered tcp transport module.
    > lib80211: common routines for IEEE802.11 drivers Power Management for TI OMAP3.
    > mmc0: host does not support reading read-only switch. assuming write-enable.
    > mmc0: new SD card at address 0002
    > pm_dbg_init()
    > mmcblk0: mmc0:0002 SDM 1.87 GiB
    > SmartReflex driver initialized
    > Disabling unused clock "gpt2_ick"
    > Disabling unused clock "gpio2_dbck"
    > Disabling unused clock "gpio5_dbck"
    > Disabling unused clock "gpio6_dbck"
    > Disabling unused clock "gpt2_fck"
    > Disabling unused clock "sad2d_ick"
    > Disabling unused clock "dpll5_ck"
    > clock: dpll5_ck failed transition to 'locked'
    > Disabling unused clock "dpll4_m6x2_ck"
    > Disabling unused clock "dpll3_m3x2_ck"
    > Disabling unused clock "sys_clkout1"
    > mmcblk0: p1 p2
    > VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
    > FIXME: no omap_set_dma_color_mode on 24xx DMA transaction error with device 0
    > Console: switching to colour frame buffer device 100x30 omapdss DPI: Could not find exact pixel clock. Requested 21800 kHz, got 21600 kHz
    > GPIO-199 autorequested
    > omapdss DPI error: display already enabled omap_voutDisplay already enabled omapdss DPI error: display already enabled omap_voutDisplay already enabled omap_voutBuffer Size = 4096000
    > omap_vout: registered and initialized video device 0 [v4l2] omap_voutBuffer Size = 4096000
    > omap_vout: registered and initialized video device 1 [v4l2] omap_voutdisplay->updated
    > imx046 2-001a: model id detected 0x46 mfr 0xb, rev# 0x2
    > imx046 2-001a: imx046 chip version 0x02 detected video4linux video5: video5 is now omap3/imx046//
    > lv8093 Lens HW detected
    > video4linux video5: video5 is now omap3/imx046/lv8093/
    > lv8093 2-0072: Registered lv8093 as V4L2 device.
    > mmc1: new MMC card at address 0001
    > Registered lv8093 as i2c device.
    > mmcblk1: mmc1:0001 SDM032 30.6 MiB
    > mmcblk1:<6>twl4030_rtc twl4030_rtc: setting system clock to 2000-01-01 00:01:20 UTC (946684880) ma``i!0 `adpqihe aqahe aahede ``maa `aa`Mhoib, 

     

     

    Thanks n Regards :

    Umang Gupta