This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Selecting DVO1 (Vout-1) instead of HDMI



Hi,

I am working on DM-385  and using IPNC_RDK 3.80.00.

I am getting sensor's frame data on HDMI but I want the data on Vout-1 port but in HD_VPSS block diagram ( TRM, section- HDVPSS) it is showing the DVO1 output is coming from HDMI only.It means there are two output coming from encoder HDMI
a.)One through hdmi xmt
b.)Vout-1

Can anyone explain this ?

On software side what changes I have to made to select DVO1 (Vout 1 port) so that my  sensor data will go to Vout-1 port ?

Regards,
Hardik