Hi,
I am using TMS320C6748 LCDK and Starterware 1_20_03_03. I am trying to configure the Starter ware example code usb_host_msc.c to use USB1.1 instead of USB OTG. I tried to modify SYS_INT_USB0 to SYS_INT_USB1_HCINT in the code below and changing USB0HostIntHandler accordingly. I am almost sure that is not enough but I wanted to get some suggestions from anybody who was successfull in configuring USB1.1.
All I need is for it is to detect a mass storage device on USB 1.1 the same way it already does on USB OTG.
--Thank You
static void ConfigureIntUSB(void) { #ifdef _TMS320C6X IntDSPINTCInit(); IntRegister(5, USB0HostIntHandler); IntEventMap(5, SYS_INT_USB0); IntEnable(5); IntGlobalEnable(); ..... }