This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

suggest the suitable MSP family microncontroller



Hi,

We have planned to make use of one of Ti's MSP family microcontroller. Our project demands for following requirements,

1)Number of 12 bit ADC channels required : 12

2)Number of PWM required : 4

3)160 segment LCD display.

4)number GPIO pins required :20 Pins

Note: please make sure that LCD interfacing pins are not multiplexed with analog pins(ADC channels ) or PWM pins.

Please suggest suitable microcontroller for the above requiments in MSP family or any other family if not available in same.

Regards,

Sunil