This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

static created timer not available

Other Parts Discussed in Thread: SYSBIOS

 

Hi all,

         I meet a problem when using C6678.

My project use SYS/BIOS 6.35.1.29, XDCTools version is 3.25.0.48.

I build my project sucessfully. The .out file can be loaded at Core0-3.But it can not

be loaded at Core4-7. I get some information like this at Core4-7:

[C66xx_4] ti.sysbios.timers.timer64.Timer: line 551: assertion failure: A_notAvailable: static created timer not availablexdc.runtime.Error.raise: terminating execution

The first picture showed the .out file is sucessfully loaded at Core2. And all startup state is DONE.

The second picutre showed It is failed to load the same .out file at Core4. Several startup state is NOT DONE.

Thanks a lot.