Hi Experts,
I am using AM335x EVM starter kit with SDK 6.0.
I tried to write the MLO and uboot image into NAND flash as shown in the link http://processors.wiki.ti.com/index.php/Linux_Core_U-Boot_User%27s_Guide
When I tried to issue the command load in the u-boot terminal then it is displayed as u-boot command not available. How to do the same using the SDK 6.0 u-boot ?