Other Parts Discussed in Thread: TMS320C6455
Hi
A customer is re-spinning an existing DSP board with TMS320C6455 on it. They are grounding RSV07 pin as we do not use EMAC RGMII interface (per recommendation from datasheet). Will this cause a problem running JTAG as this pin is specified HIGN in the BSDL file?
Accoring to BSDL, this pin must be at the specified level: high. The manufacturer puts this in the BSDL as a compliance enable.Some or all of the boundary scan functionality will not be available unless the compliance enables are met. Unfortunately, the manufacturer does not specify what boundary scan functionality will not be available if the compliance enables are not met (typical of most devices/compliance enables/manufacturers).
Cusotmer still have problems in their current design running DSP JTAG chain in conjunction with other JTAG chains. We have to run the DSP chain separately by itself. Is ti possible to get a BSDL file with RSV07 pin tied low simulating behavior we have? (bypassing EMAC JTAG interface)