This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

nand boot

hi   all,

I want to use boot programs from nand.

I use ibl to boot programs from nand successfully.Now, I want to boot program drectily from nand.Thanks for anyone can help me realize the idea. 

I  use the TI c6678 EVM board.

Thanks.

  • Hi Huajin,

    Please provide your DSP C6678 chip version? (Eg: PG1.0 or PG2.0)

    The PLL fix implemented for PG2.0 was to fix an issue w/ PLL initialization only, on 1.0 this required the use of an I2C ROM to configure the PLL properly for the initial configuration.

    For more information refer "Advisory 8 Multiple PLLs May Not Lock After Power-on Reset Issue" on C6678 Silicon Errata document.

    http://www.ti.com/lit/sprz334

    Thanks,

  • huanjin yuan,

    Direct boot from NAND is not supported in C6678 devices. Please refer to section 2.5 of the device datasheet to look at supported boot modes. The support for direct NAND boot using boot ROM was introduced on C6657 in Keystone I device family.

    Hence in order to boot using NAND on C6678, you would need to use IBL code.


    Regards,

    Rahul