This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-RTOS example tcpEcho - EK-TM4C1294XL nor run when power applied - run when debug

Hello

I have a little question, this is the second TI-RTOS project (first already running on tiva 123 MCU target product).

This time code is ready to be moved to the target hardware but how to make it running when power is applied. It only seem to start the code execution when I start the debug session and code keep running when debugger is disconnected. But when I reapplay the power device wont start.

I have observed that behavior even with tcpEcho example with no changes to code. Import, debug and everything runs ok. But when I take the board and apply the power only (via debug or OTG - jumper selection) the code wont start. When working with TI-RTOS for Tiva 123 that wasn't the case.

I don't even know where to start solving the problem, is it the linker script? I have changed from debug to release and used the same linker script no help.

Regards

Patrick