Hi, TIer
I'm using DM8168 with RDK3.0
In my usecase, there are 4 channels to be encoded:
1. Camera-0 channel, via Capture LINK,
2. PCIe video channel, via IPCFrameIn/Out LINK,
3. Swms-0 channel, the output of Swms LINK,
4. Swms-0 sub channel, the output of SwmsLINK----ScalarLINK,
M3-video core will pause outputing encoded stream when A8 load upto approximately 90%,
If the load drop down to a normal level, e.g 10-30%,
when PCIe channel disconnected, the core will keep the state,
when PCIe channel connected, the core will recover.
What causes this issue, and how to fix it?
Best Regards!