This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138LCDK SATA test

Works in an annex.
Project is in accordance with the DM8168's SATA test procedure modified from.
CCS5.3, OMAPL138LCDK development board, 560 emulator.
Pick 500G SATA2 hard drive, then use a computer hard drive cable, computer power supply, SATA cable connected to the board.
Program to run while ((sataRegs-> P0SSTS & AHCI_PxSCTL_PxSSTS_DET)! = 0x3).

Use native linux SD card within the hard disk can not connect.3730.3036.sata.rar