I am a newbie to the EVMK2H board, and am working to benchmark the performance of it by using a number of industry-recognized benchmarks (EEMBC). This is an evaluation exercise, so we are working to simply compile benchmark code on the processor and run it. We are not working to evaluate the DSP processing at this time, just the ARM processor. We are remoting to the processor via Putty (like the Terra Term), copying code files there and make file, completing the compile and running the resultant executable on the core. So, we are not using the MCSDK or CCS at present. Just using the resident Linux on the board. We are trying to figure out how to run the different benchmarks on a selection of the cores. So, how do we simply remote into an individual core and execute our process there? In Terra Term, how do you navigate to access the different cores? Is there an address map of the cores?
Thanks.