This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

zoom2 board not working

 

Zoom2 board boots up , and hangs in the middle of kernel , the logs are as such:-

U-Boot 1.1.4-dirty (Mar 27 2009 - 11:27:11)

 

OMAP3430-GP rev 2, CPU-OPP2 L3-165MHz

OMAP3430LAB 0.1 Version + mDDR (Boot NAND)

DRAM: 256 MB

NAND:512 MiB

 

Reading data from 0xdf800 -- 100% complete.

In: serial

Out: serial

Err: serial

Hit any key to stop autoboot: 0

 

2792352 bytes read

## Booting image at 80000000 ...

Image Name: Linux-2.6.29.6-omap1

Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 2792288 Bytes = 2.7 MB Load Address: 80008000 Entry Point: 80008000 Verifying Checksum ... OK OK

 

Starting kernel ...

 

Uncompressing

Linux.............................................................................................

Linux version 2.6.29.6-omap1 (root@deepak) (gcc version 4.3.2 (Sourcery

G++ Lite 2008q3-72) ) #16 PREEMPT Thu J0

CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c5387f

CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache

Machine: OMAP ZOOM2 board

Memory policy: ECC disabled, Data cache writeback OMAP3430 ES3.1

SRAM: Mapped pa 0x40200000 to va 0xe3000000 size: 0x100000 Reserving 4194304 bytes SDRAM for VRAM Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024 Kernel command line: console=ttyS3,115200n8 root=/dev/mmcblk0p2 rw ip=off mem=256M devfs=mount init=/init Clocking rate (Crystal/DPLL/ARM core): 26.0/166/500 MHz GPMC revision 5.0

IRQ: Found an INTC at 0xd8200000 (revision 4.0) with 96 interrupts Total of 96 interrupts on 1 active controller OMAP34xx GPIO hardware version 2.5 PID hash table entries: 1024 (order: 10, 4096 bytes) OMAP clockevent source: GPTIMER1 at 32768 Hz

Console: colour dummy device 80x30

Dentry cache hash table entries: 32768 (order: 5, 131072 bytes) Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

Memory: 256MB = 256MB total

Memory: 249344KB available (5260K code, 779K data, 180K init) Calibrating delay loop... 498.87 BogoMIPS (lpj=1945600) Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

net_namespace: 520 bytes

regulator: core version 0.5

NET: Registered protocol family 16

MUX: setup H18_34XX_GPIO163 (0xd800219a): 0x0108 -> 0x011c

MUX: setup B24_34XX_GPIO101_OUT (0xd800211a): 0x0104 -> 0x0004

MUX: setup A24_34XX_GPIO94 (0xd800210c): 0x0007 -> 0x0104

MUX: setup C25_34XX_GPIO96 (0xd8002110): 0x0000 -> 0x0004

MUX: setup H16_34XX_SDRC_CKE0 (0xd8002262): 0x0118 -> 0x0000

MUX: setup H17_34XX_SDRC_CKE1 (0xd8002264): 0x0118 -> 0x0000 OMAP DMA hardware revision 4.0

bio: create slab <bio-0> at 0

i2c_omap i2c_omap.1: bus 1 rev3.12 at 100 kHz

twl4030: PIH (irq 7) chaining IRQs 368..375

twl4030: power (irq 373) chaining IRQs 376..383

twl4030: gpio (irq 368) chaining IRQs 384..401

twl4030_mmc_init:362

twl4030_mmc_init:377

twl4030_mmc_init:377

twl4030_mmc_init:377

MUX: setup M27_3430_MMC1_CMD (0xd8002146): 0x0118 -> 0x0000

MUX: setup P27_3430_MMC1_DAT4 (0xd8002150): 0x0018 -> 0x0118

MUX: setup P26_3430_MMC1_DAT5 (0xd8002152): 0x0018 -> 0x0118

MUX: setup R27_3430_MMC1_DAT6 (0xd8002154): 0x0018 -> 0x0118

MUX: setup AE2_3430_MMC2_CLK (0xd8002158): 0x0101 -> 0x0100

MUX: setup AG5_3430_MMC2_CMD (0xd800215a): 0x0101 -> 0x0118

MUX: setup AH5_3430_MMC2_DAT0 (0xd800215c): 0x0101 -> 0x0118

MUX: setup AH4_3430_MMC2_DAT1 (0xd800215e): 0x011c -> 0x0118

MUX: setup AG4_3430_MMC2_DAT2 (0xd8002160): 0x0009 -> 0x0118

MUX: setup AF4_3430_MMC2_DAT3 (0xd8002162): 0x0109 -> 0x0118

MUX: setup AF10_3430_MMC3_CLK (0xd80025d8): 0x001b -> 0x011a

MUX: setup AC3_3430_MMC3_CMD (0xd80021d0): 0x000b -> 0x011b

MUX: setup AE11_3430_MMC3_DAT0 (0xd80025e4): 0x0103 -> 0x011a

MUX: setup AH9_3430_MMC3_DAT1 (0xd80025e6): 0x0103 -> 0x011a

MUX: setup AF13_3430_MMC3_DAT2 (0xd80025e8): 0x0103 -> 0x011a

MUX: setup AE13_3430_MMC3_DAT3 (0xd80025e2): 0x0103 -> 0x011a

regulator: VMMC1: 1850 <--> 3150 mV normal standby

regulator: VDAC: 1800 mV normal standby

regulator: VUSB1V5: 1500 <--> 0 mV normal standby

regulator: VUSB1V8: 1800 <--> 0 mV normal standby

regulator: VUSB3V1: 3100 <--> 0 mV normal standby

regulator: VMMC2: 1850 mV normal standby

regulator: VSIM: 1800 <--> 3000 mV normal standby i2c_omap i2c_omap.2: bus 2 rev3.12 at 100 kHz i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz SCSI subsystem initialized twl4030_usb twl4030_usb: Initialized TWL4030 USB module

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Bluetooth: Core ver 2.15

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

cfg80211: Using static regulatory domain info

cfg80211: Regulatory domain: US

(start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp) (2402000 KHz - 2472000 KHz @ 40000 KHz), (600 mBi, 2700 mBm) (5170000 KHz - 5190000 KHz @ 40000 KHz), (600 mBi, 2300 mBm) (5190000 KHz - 5210000 KHz @ 40000 KHz), (600 mBi, 2300 mBm) (5210000 KHz - 5230000 KHz @ 40000 KHz), (600 mBi, 2300 mBm) (5230000 KHz - 5330000 KHz @ 40000 KHz), (600 mBi, 2300 mBm) (5735000 KHz - 5835000 KHz @ 40000 KHz), (600 mBi, 3000 mBm)

cfg80211: Calling CRDA for country: US

musb_hdrc: version 6.0, musb-dma, host, debug=0

musb_hdrc: USB Host mode controller at d80ab000 using DMA, IRQ 92 musb_hdrc musb_hdrc: MUSB HDRC host driver musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1 usb usb1: configuration #1 chosen from 1 choice hub 1-0:1.0: USB hub found hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 2048 (order: 1, 8192 bytes) TCP established hash table entries: 8192 (order: 4, 65536 bytes) TCP bind hash table entries: 8192 (order: 3, 32768 bytes)

TCP: Hash tables configured (established 8192 bind 8192) TCP reno registered

NET: Registered protocol family 1

zoom2_wifi_init: start

omap-iommu omap-iommu.1: isp registered

NetWinder Floating Point Emulator V0.97 (double precision)

ashmem: initialized

VFS: Disk quotas dquot_6.5.2

Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

JFFS2 version 2.2. (NAND)  © 2001-2006 Red Hat, Inc.

yaffs Jan 21 2010 12:08:16 Installing.

msgmni has been set to 487

alg: No test for stdrng (krng)

io scheduler noop registered

io scheduler anticipatory registered (default) io scheduler deadline registered io scheduler cfq registered OMAP DSS rev 2.0 OMAP DISPC rev 3.0 OMAP VENC rev 2

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654

serial8250.0: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654

serial8250.0: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654

serial8250.0: ttyS3 at MMIO 0x10000000 (irq = 262) is a ST16654 console [ttyS3] enabled

brd: module loaded

loop: module loaded

eth0 (smc911x): not using net_device_ops yet

eth0: LAN9221 (rev 0) at 0x8000000 IRQ 318

eth0: Ethernet addr: 00:00:00:00:82:a8

Broadcom 43xx driver loaded [ Features: , Firmware-ID: FW13 ] Broadcom 43xx-legacy driver loaded [ Features: ID, Firmware-ID: FW10 ]

usbcore: registered new interface driver rt73usb Linux video capture interface: v2.00 omap-previewer omap-previewer: omap-previewer: Registered preview wrapper omap-iommu omap-iommu.1: isp: version 1.1 i2c /dev entries driver Driver 'sd' needs updating - please use bus_type methods omap2-nand driver initializing NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron NAND 512MiB 1,8V 16-bit) Creating 7 MTD partitions on "omap2-nand.0":

0x000000000000-0x000000080000 : "X-Loader-NAND"

0x000000080000-0x000000100000 : "U-Boot-NAND"

0x000000100000-0x000000140000 : "Boot Env-NAND"

0x000000140000-0x000000540000 : "Kernel-NAND"

0x000000540000-0x000010540000 : "system"

0x000010540000-0x000014540000 : "userdata"

0x000014540000-0x000018540000 : "cache"

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage USB Mass Storage support registered.

udc: OMAP UDC driver, version: 4 October 2004 (iso) (dma) android init

mice: PS/2 mouse device common for all mice

input: TWL4030 Keypad as

/devices/platform/i2c_omap.1/i2c-adapter/i2c-1/1-004a/twl4030_keypad/input/input0

i2c_omap i2c_omap.2: Transmit error

synaptics_ts_probe: Product Major Version 1

synaptics_ts_probe: Product Minor Version 5

synaptics_ts_probe: product property 2

synaptics_ts_probe: device control 81

synaptics_ts_probe: interrupt enable 3

synaptics_ts_probe: 0xe0: 1 1 1 2 1 5 0 0

synaptics_ts_probe: Sensor properties 601

synaptics_ts_probe: max_x 7515, max_y 4667

synaptics_ts_probe: inactive_x 0 0, inactive_y 0 0

synaptics_ts_probe: snap_x 0-0 0-0, snap_y 0-0 0-0

input: synaptics-rmi-touchscreen as /devices/virtual/input/input1

synaptics_ts_probe: Start touchscreen synaptics-rmi-touchscreen in interrupt mode twl4030_rtc twl4030_rtc: rtc core: registered twl4030_rtc as rtc0 Driver for 1-wire Dallas network protocol.

omap_hdq omap_hdq.0: OMAP HDQ Hardware Rev 0.5. Driver in Interrupt mode w1_master_driver w1 bus master: Family 1 for 01.000000000000.3d is not registered.

Android battery driver installed

OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec

Bluetooth: Virtual HCI driver ver 1.2

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCI H4 protocol initialized

Bluetooth: HCI BCSP protocol initialized

Bluetooth: HCILL protocol initialized

Bluetooth: Broadcom Blutonium firmware driver ver 1.2

usbcore: registered new interface driver bcm203x

Bluetooth: Digianswer Bluetooth USB driver ver 0.10

usbcore: registered new interface driver bpa10x

Bluetooth: BlueFRITZ! USB driver ver 1.2

usbcore: registered new interface driver bfusb

Bluetooth: Generic Bluetooth USB driver ver 0.5

usbcore: registered new interface driver btusb

Bluetooth: Generic Bluetooth SDIO driver ver 0.1

cpuidle: using governor ladder

cpuidle: using governor menu

regulator: Unable to get requested regulator: vmmc_aux

regulator: Unable to get requested regulator: vmmc

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

logger: created 64K log 'log_main'

logger: created 256K log 'log_events'

logger: created 64K log 'log_radio'

Advanced Linux Sound Architecture Driver Version 1.0.18a.

No device for DAI twl4030

No device for DAI twl4030 Voice

No device for DAI omap-mcbsp-dai-0

No device for DAI omap-mcbsp-dai-1

No device for DAI omap-mcbsp-dai-2

No device for DAI omap-mcbsp-dai-3

No device for DAI omap-mcbsp-dai-4

Zoom2 SoC init

TWL4030 Audio Codec init

asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok

asoc: twl4030 Voice <-> omap-mcbsp-dai-1 mapping ok ALSA device list:

#0: Zoom2 (twl4030)

TCP cubic registered

Initializing XFRM netlink socket

NET: Registered protocol family 17

NET: Registered protocol family 15

Bluetooth: L2CAP ver 2.13

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO (Voice Link) ver 0.6

Bluetooth: SCO socket layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

lib80211: common routines for IEEE802.11 drivers Power Management for TI OMAP3.

mmc0: host does not support reading read-only switch. assuming write-enable.

mmc0: new SD card at address 0002

pm_dbg_init()

mmcblk0: mmc0:0002 SDM 1.87 GiB

SmartReflex driver initialized

Disabling unused clock "gpt2_ick"

Disabling unused clock "gpio2_dbck"

Disabling unused clock "gpio5_dbck"

Disabling unused clock "gpio6_dbck"

Disabling unused clock "gpt2_fck"

Disabling unused clock "sad2d_ick"

Disabling unused clock "dpll5_ck"

clock: dpll5_ck failed transition to 'locked'

Disabling unused clock "dpll4_m6x2_ck"

Disabling unused clock "dpll3_m3x2_ck"

Disabling unused clock "sys_clkout1"

mmcblk0: p1 p2

VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1

FIXME: no omap_set_dma_color_mode on 24xx DMA transaction error with device 0

Console: switching to colour frame buffer device 100x30 omapdss DPI: Could not find exact pixel clock. Requested 21800 kHz, got 21600 kHz

GPIO-199 autorequested

omapdss DPI error: display already enabled omap_voutDisplay already enabled omapdss DPI error: display already enabled omap_voutDisplay already enabled omap_voutBuffer Size = 4096000

omap_vout: registered and initialized video device 0 [v4l2] omap_voutBuffer Size = 4096000

omap_vout: registered and initialized video device 1 [v4l2] omap_voutdisplay->updated

imx046 2-001a: model id detected 0x46 mfr 0xb, rev# 0x2

imx046 2-001a: imx046 chip version 0x02 detected video4linux video5: video5 is now omap3/imx046//

lv8093 Lens HW detected

video4linux video5: video5 is now omap3/imx046/lv8093/

lv8093 2-0072: Registered lv8093 as V4L2 device.

mmc1: new MMC card at address 0001

Registered lv8093 as i2c device.

mmcblk1: mmc1:0001 SDM032 30.6 MiB

mmcblk1:<6>twl4030_rtc twl4030_rtc: setting system clock to 2000-01-01 00:01:20 UTC (946684880) ma``i!0 `adpqihe aqahe aahede ``maa `aa`Mhoib, `  

Does any body have a workaround for this..

let me know

Vandana