Hi,
My platform was TI8148, and I create an BIOS project for cortex-A8, and try to power on DSP from cortex-A8, but it's failure as I can not confgure PRCM module from my BIOS project. u-boot or GEL file can done this success, I don't know why, who can help me.
Attach was my test project which set pll in an BIOS project. It would hang up at file main.c line 131. I also make another test that I make XDC Startup modules firstFxns call ipnc_ff_pll_init, it's pass, but if I set ipnc_ff_pll_init to lastFxns of Startup, it's also not work.1055.test_bios_pll.zip