This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3725 Power-up sequence

Hello.


I need to know the exact timing of the power-up sequence (or at least the ballpark) but I can't find these numbers anywhere in the technical documentation. The reason I need to know this is, I'm planning to connect a parallel NOR-flash device to the processor, and the flash IC I've chosen requires at least 30us of asserted reset after its VCC has ramped up. Considering how the two devices work tightly in pair, it is only logical that I should use the processor reset for this purpose. The question is, can I? And if I can, which one? Power-On Reset or Warm Reset?

Thank you