Other Parts Discussed in Thread: AM3352, AM3517
I have a customer asking of the AM3352 supports Synchronous NAND (Micron G08ABCBBH1-12IT:B).
I checked the forum postings and found the AM3517 does not. I assume it is the same for the AM335x. Additionally, I found in the AM335x TRM the following statements:
7.1.3.3.8.2.1 Supported Devices
The access protocol of each chip-select can be independently specified through the GPMC_CONFIG1_i[11-10] DEVICETYPE parameter for:
• Random-access synchronous or asynchronous memory like NOR flash, SRAM
• NAND flash asynchronous devices
For more information about the NAND flash GPMC basic programming model and NAND support, see Section 7.1.3.3.12 and Section 7.1.3.3.12.1.
I think the answer is "no" it does not support synchronous NAND, but I would like for you to confirm this.