This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5515 GPIO output



Hi,

I want to set GPIO-18 and GPIO-20 on output mode , control high/low.

The code cannot work normally for GPIO-18 and GPIO-20.

Please guide me GPIO setting.

CPU:C5515

Board:costom

==================================

typedef enum {

/** GPIO as i/p */
CSL_GPIO_DIR_INPUT = 0,
/** GPIO as o/p */
CSL_GPIO_DIR_OUTPUT = 1

} CSL_GpioDirection;

typedef enum {
/** Gpio pin 18 */
CSL_GPIO_PIN18 = 18,

/** Gpio pin 20 */
CSL_GPIO_PIN20 = 20,
} CSL_GpioPinNum;

main()

{

gpioIoDir = 
(((Uint32)CSL_GPIO_DIR_OUTPUT)<<CSL_GPIO_PIN18) |
(((Uint32)CSL_GPIO_DIR_OUTPUT)<<CSL_GPIO_PIN20);

gpioInit(gpioIoDir, 0x20600340, 0x00600340);

dbgGpioWrite(1, 18);
dbgGpioWrite(0, 18);

dbgGpioWrite(1, 20);
dbgGpioWrite(0, 20);

}

//// gpio init area

Int16 gpioInit(
Uint32 ioDir,
Uint32 intEn,
Uint32 intEdg
)
{
CSL_Status status;
CSL_GpioConfig config;

/* Open GPIO module */
hGpio = GPIO_open(&gGpioObj, &status);
if ((hGpio == NULL) || (status != CSL_SOK))
{
return GPIOCTRL_OPEN_FAIL;
}

/* Reset GPIO module */
status = GPIO_reset(hGpio);
if (status != CSL_SOK)
{
return GPIOCTRL_RESET_FAIL;
}

/* Configure GPIO module */
config.GPIODIRL = ioDir & 0xFFFF;
config.GPIODIRH = ioDir >> 16;
config.GPIOINTENAL = intEn & 0xFFFF;
config.GPIOINTENAH = intEn >> 16;
config.GPIOINTTRIGL = intEdg & 0xFFFF;
config.GPIOINTTRIGH = intEdg >> 16;
status = GPIO_config(hGpio, &config);
if (status != CSL_SOK)
{
return GPIOCTRL_CFG_FAIL;
}

return GPIOCTRL_SOK;
}

GPIO_Handle GPIO_open (
CSL_GpioObj* GpioObj,
CSL_Status * status
)
{
GPIO_Handle hGpio = (CSL_GpioObj*)NULL;
/* For Invalid handle */
if(NULL == GpioObj)
{
*status = CSL_ESYS_BADHANDLE;
return NULL;
}

GpioObj->numPins = CSL_GPIO_NUM_PIN;
/* Base Address of GPIO Registers */
GpioObj->baseAddr = CSL_GPIO_REGS;
hGpio = (GPIO_Handle)GpioObj;
*status = CSL_SOK;

return hGpio;
}

CSL_Status GPIO_reset (
GPIO_Handle hGpio
)
{
/* For Invalid handle */
if(NULL == hGpio)
{
return CSL_ESYS_BADHANDLE;
}
/* Reset the GPIO Registers */
hGpio->baseAddr->IOINTEN1 = CSL_GPIO_IOINTEN1_RESETVAL ;
hGpio->baseAddr->IOINTEN2 = CSL_GPIO_IOINTEN2_RESETVAL ;

hGpio->baseAddr->IOINTFLG1 = (Uint16)(~CSL_GPIO_IOINTFLG1_RESETVAL);
hGpio->baseAddr->IOINTFLG2 = (Uint16)(~CSL_GPIO_IOINTFLG2_RESETVAL);

hGpio->baseAddr->IOINTEDG1 = (Uint16)(CSL_GPIO_IOINTEDG1_RESETVAL);
hGpio->baseAddr->IOINTEDG2 = (Uint16)(CSL_GPIO_IOINTEDG2_RESETVAL);

hGpio->baseAddr->IODIR1 = CSL_GPIO_IODIR1_RESETVAL;
hGpio->baseAddr->IODIR2 = CSL_GPIO_IODIR2_RESETVAL;

hGpio->baseAddr->IOOUTDATA1 = CSL_GPIO_IOOUTDATA1_RESETVAL;
hGpio->baseAddr->IOOUTDATA2 = CSL_GPIO_IOOUTDATA2_RESETVAL;

return CSL_SOK;
}

////////

Int16 dbgGpioWrite(Uint16 *gpioIutputValue, Uint16 pinNum)
{
CSL_Status status;
Int16 ret = GPIOCTRL_SOK;

status = (CSL_Status)GPIO_write((GPIO_Handle)hGpio, (CSL_GpioPinNum)pinNum, (Uint16)gpioIutputValue);

if(status != CSL_SOK)
{
ret = GPIOCTRL_WRITE_FAIL;
}

return ret;
}

CSL_Status GPIO_write (
GPIO_Handle hGpio,
CSL_GpioPinNum pinNum,
Uint16 buffer
)
{
Uint16 pin;
/* For Invalid handle */
if(NULL == hGpio)
{
return CSL_ESYS_BADHANDLE;
}
/* For wrong Pin Index */
if((CSL_GPIO_PIN31 < pinNum)||(pinNum < CSL_GPIO_PIN0))
{
return CSL_ESYS_INVPARAMS;
}
/* For wrong o/p write data */
if(buffer != GPIO_DRIVE_HIGH && buffer != GPIO_DRIVE_LOW)
{
return CSL_ESYS_INVPARAMS;
}

if(pinNum < CSL_GPIO_PIN16)
{
/* Lower Sixteen GPIO Pin - 0 to 15 GPIO pin */
pin = pinNum;
CSL_FINSR (hGpio->baseAddr->IOOUTDATA1,pin,pin,buffer);
}
else
{
/* Upper Sixteen 16 to 31 GPIO Pin */
pin = pinNum - CSL_GPIO_PIN16;
CSL_FINSR(hGpio->baseAddr->IOOUTDATA2,pin,pin,buffer);
}
return CSL_SOK;
}

  • Hi,

    Please refer or use the CSL GPIO example code - " gpio_Output_Pin_Example.c " (CSL_GPIO_OutputPinExample).

    This example code tests the GPIO(General Purpose Input Output) pin functionality as output pin. This example also verifies configuring the CSL GPIO module.C5535/C5515/C5517 DSPs have 32 GPIO pins which can be configured as input or output. Output functionality of the GPIO pin is verified by this test.During this test GPIO Pin is configured as output pin. A value is written to GPIO pin and verified by reading it back.

    Link - sprc133

    Hope the above information helps.

    Regards

     Vasanth