Hi all
I am using TI platform for AM335x, with Am335x EVM Board, download SDK from the following URL
http://software-dl.ti.com/sitara_linux/esd/AM335xSDK/06_00_00_00/index_FDS.html
I'm trying to enable the timer2~7 using the following code, and the result shows the timer3 and timer6 couldn't enable succeed (cmper->timer3clkctrl & cmper->timer6clkctrl) but timer2,4,5,7 could . I feel confused, does anyone know what's wrong with my code :-(
/*
* Force power domain wake up transition
* Ensure that the corresponding interface clock is active before
* using the peripheral
*/
static void power_domain_wkup_transition(void)
{
writel(PRCM_FORCE_WAKEUP, &cmper->l3clkstctrl);
writel(PRCM_FORCE_WAKEUP, &cmper->l4lsclkstctrl);
writel(PRCM_FORCE_WAKEUP, &cmwkup->wkclkstctrl);
writel(PRCM_FORCE_WAKEUP, &cmper->l4fwclkstctrl);
writel(PRCM_FORCE_WAKEUP, &cmper->l3sclkstctrl);
//Enable the domain power state for Timer2~7
writel(0x1 << 13, &cmper->l4lsclkstctrl);/*Timer 7*/
writel(0x1 << 28, &cmper->l4lsclkstctrl);/*Timer 6*/
writel(0x1 << 27, &cmper->l4lsclkstctrl);/*Timer 5*/
writel(0x1 << 16, &cmper->l4lsclkstctrl);/*Timer 4*/
writel(0x1 << 15, &cmper->l4lsclkstctrl);/*Timer 3*/
}
/*
* Enable the peripheral clock for required peripherals
*/
static void enable_per_clocks(void)
{
/* Enable the control module though RBL would have done it*/
writel(PRCM_MOD_EN, &cmwkup->wkctrlclkctrl);
while (readl(&cmwkup->wkctrlclkctrl) != PRCM_MOD_EN)
;
/* Enable the module clock */
writel(PRCM_MOD_EN, &cmper->timer7clkctrl);
while (readl(&cmper->timer7clkctrl) != PRCM_MOD_EN)
;
/* Select the Master osc 24 MHZ as Timer7 clock source */
writel(0x1, &cmdpll->clktimer7clk);
/* Enable the module clock */
writel(PRCM_MOD_EN, &cmper->timer2clkctrl);
while (readl(&cmper->timer2clkctrl) != PRCM_MOD_EN)
;
/* Select the Master osc 24 MHZ as Timer2 clock source */
writel(0x1, &cmdpll->clktimer2clk);
/* Enable the module clock */
writel(PRCM_MOD_EN, &cmper->timer3clkctrl);
while (readl(&cmper->timer3clkctrl) != PRCM_MOD_EN)
;
/* Select the Master osc 24 MHZ as Timer3 clock source */
writel(0x1, &cmdpll->clktimer3clk);
/* Enable the module clock */
writel(PRCM_MOD_EN, &cmper->timer4clkctrl);
while (readl(&cmper->timer4clkctrl) != PRCM_MOD_EN)
;
/* Select the Master osc 24 MHZ as Timer4 clock source */
writel(0x1, &cmdpll->clktimer4clk);
/* Enable the module clock */
writel(PRCM_MOD_EN, &cmper->timer5clkctrl);
while (readl(&cmper->timer5clkctrl) != PRCM_MOD_EN)
;
/* Select the Master osc 24 MHZ as Timer5 clock source */
writel(0x1, &cmdpll->clktimer5clk);
/* Enable the module clock */
writel(PRCM_MOD_EN, &cmper->timer6clkctrl);
while (readl(&cmper->timer6clkctrl) != PRCM_MOD_EN)
;
/* Select the Master osc 24 MHZ as Timer6 clock source */
writel(0x1, &cmdpll->clktimer6clk);
....
....
....
}
/*
* Configure the PLL/PRCM for necessary peripherals
*/
void pll_init()
{
/* Start at 550MHz, will be tweaked up if possible. */
mpu_pll_config(MPUPLL_M_300);
core_pll_config(OPP_50);
per_pll_config();
/* Enable the required interconnect clocks */
enable_interface_clocks();
/* Power domain wake up transition */
power_domain_wkup_transition();
/* Enable the required peripherals */
enable_per_clocks();
}