Other Parts Discussed in Thread: DM3730
Hi all
I am trying to use gpio 129 and doing this
I am trying to understand the configuration of extended drain pins. What I understood so far is that there are two registers
CONTROL_PBIAS_LITE and CONTROL_WKUP_CTRL
From my understanding we can get two kinds of outputs from these gpios, 3.0 volts and 1.8 volts by changing vmode bit.
I am reading first the PBIAS_LITE register and the value it gives is 0x8387. So SIM_VDDS is 3.0 volt
SIM_VDDS is stable and VMODE1 is giving 3.0 volts.
Now I am writing same bit value in CONTROL_WKUP_CTRL in GPIO_IO_PWRDNZ to enable gpio129 associated buffers.
I am not getting 3.0 volt on the 129 pin. Why?