Other Parts Discussed in Thread: AM1808, DA8XX
Dar all,
i succesffully had USB working on kernel 3.17 on a AM1808 based board.
After reboot, with key inserted, automount detect the key and mount it correctly.
Once removed, i see a message as:
[root@test local]# usb 1-1: USB disconnect, device number 2 FAT-fs (sda1): unable to read boot sector to mark fs as dirty
But once the key is re-inserted, i don't see it detected nor mounted.
also lsusb doesn't show the usb pen anymore.
Could i have some issue with udev / automount or menuconfig ?
Thanks