This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB0 host mode am335x



Hi,

We have an AM335x Starter Kit and we've been trying some modifications in order to use USB0 as host. Here what we did:

1- Remove usb hub

2- Connect DP and DM to another connector (where we will plug the devices) and GND of course

3- Grounded USB0_ID

4- Supply 5V to USB0_VBUS

5- Install gadget driver in Linux (like g_mass_storage to use a pendrive or  g_serial to use a cdc device).

But after doing that the processor can't recognize any device attached to USB0; dmesg and lsusb show messages as if the hub were still connected.

What should we do? Is that a s/w issue? Should we make another modification and recompile the kernel?

Regards,

Fernando