This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Performance metrics / benchmarks on C6670



Hello,

I am doing some basic performance testing on the EVM6670LE platform. I've got a small app that allows commands to be issued through the UART and can run the whetstone test. I've attached the project for reference. In the current configuration with optimization level 3. With these settings, running on a single core, the whetstone test reports  the following:

Loops: 100000, Iterations: 1, Duration: 45 sec. C Converted Double Precision Whetstones: 222.2 MIPS

Questions:

1. Is this a valid test?

2. Is this number reasonable? 

3. Is there a better benchmark with freely available source code?

Thanks,

Dave

3365.uart.zip