Other Parts Discussed in Thread: CCSTUDIO
When I try to run lab2 I get an error message that the dsk6416.h file has not been located.the file is included in the documents folder,I've manually added it to the project folder but it still doesn't work.
I've even added the directory of the header file in the build options section under linker but it still doesn't work.
here's the error message:
------------------------------ lab2.pjt - Debug ------------------------------
[lab2.cdb] "C:\CCStudio_v3.1\plugins\bios\gconfgen" lab2.cdb
[Block_Sine.c] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -g -fr"C:/CCStudio_v3.1/examples/dsk6416/bsl/lab2/Debug" -d"_DEBUG" -mv6400 -@"../../../CCStudio_v3.1/examples/dsk6416/bsl/lab2/Debug.lkf" "Block_Sine.c"
[Lab2.c] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -g -fr"C:/CCStudio_v3.1/examples/dsk6416/bsl/lab2/Debug" -d"_DEBUG" -mv6400 -@"../../../CCStudio_v3.1/examples/dsk6416/bsl/lab2/Debug.lkf" "Lab2.c"
"Lab2.c", line 1: fatal error: could not open source file "dsk6416.h"
1 fatal error detected in the compilation of "Lab2.c".
Compilation terminated.
>> Compilation failure
[lab2cfg.s62] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -g -fr"C:/CCStudio_v3.1/examples/dsk6416/bsl/lab2/Debug" -d"_DEBUG" -mv6400 -@"../../../../CCStudio_v3.1/examples/dsk6416/bsl/lab2/Debug.lkf" "lab2cfg.s62"
[lab2cfg_c.c] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -g -fr"C:/CCStudio_v3.1/examples/dsk6416/bsl/lab2/Debug" -d"_DEBUG" -mv6400 -@"../../../../CCStudio_v3.1/examples/dsk6416/bsl/lab2/Debug.lkf" "lab2cfg_c.c"
Build Complete,
1 Errors, 0 Warnings, 0 Remarks.