When I tried to build the kernel, make ...defconfig, make ...menuconfig, I found the default CPU is Davinc, not OMAP, and when I choose OMAP, the new kernel cannot boot from NFS.
Also, when I want to build the SDK, CMEM for example, the default configure file "Rules.make" is still Davinc, not OMAP. Why?
All the files like kernel, LSP , SDK are based on OMAP in addition.
Thank you!