Other Parts Discussed in Thread: SYSBIOS
Hello,
I try to find a way to avoid SYS/BIOS generating a specific INT vector for the 64x+ DSP. The CCS v6 and SYS/BIOS 6.40.1.15 generate a section named .vecs with all the vectors defined (the section size is 0x200 bytes). I use a custom communication kernel which uses the INT4 and this vector must be kept as is and must not be managed by SYS/BIOS. I do not found any way to keep the original vector as is even if this INT is not used or declared in SYS/BIOS. Any suggestion?
Thank.