Other Parts Discussed in Thread: AM1808, OMAP-L138
I have am AM437x EVM and want to try out booting from the ethernet port. That is I wish to load the u-boot SPL, u-boot and Linux via ethernet.
I have set the SW11 and SW12 to what I think are the correct values (sysboot 0-4 = 11100b for emac1 and sysboot5=1 for RGMII)
I have the RJ45 (J18) connected directly to my laptop and on power up or reset I see no network traffic.
I assume that when SW11 and SW12 switches are 'on' it selects 0 on the sysboot pin