This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AER control bitfield masks



Hi

In the AER 17.0.0.0 API documentation, bits 11 and 12 in control bitfield 1 are defined as:

        11         1       Keep clipper during double talk
                   0       Remove clipper completely during double talk        
        12                 RESERVED  

However the corresponding masks are defined as:

#define aer_CTL1_BIT_11_RESERVED 0x0800 /**< reserved */
#define aer_CTL1_RESET_PARAMS 0x1000 /**< reset config. params */

The mask seems to contradict the API, what enables are assigned to these bits?

Thanks,

Simon