Other Parts Discussed in Thread: TLV320AIC3204
Hi,
I have a problema sending data via I2S with TLV320AIC3204.
I have configured audio codec with an input in IN1R as:
/* Configure AIC3204 */
AIC3204_rset( 0, 0x00 );
// Select page 0
AIC3204_rset( 1, 0x01 );
// Reset codec
AIC3204_rset( 0, 0x01 );
// Point to page 1
AIC3204_rset( 1, 0x08 );
// Disable crude AVDD generation from DVDD
AIC3204_rset( 2, 0x00 );
// Enable Analog Blocks
// PLL and Clocks config and Power Up
AIC3204_rset( 0, 0x00 );
// Select page 0
AIC3204_rset( 27, 0x00 );
// BCLK and WCLK is set as i/p to AIC3204(Slave)
AIC3204_rset( 4, 0x07 );
// PLL setting: PLLCLK <- BCLK and CODEC_CLKIN <-PLL CLK
AIC3204_rset( 6, 0x20 );
// PLL setting: J=32
AIC3204_rset( 7, 0 );
// PLL setting: HI_BYTE(D = 0)
AIC3204_rset( 8, 0 );
// PLL setting: LO_BYTE(D) = 0
// For 48 KHz sampling
AIC3204_rset( 5, 0x92 );
// PLL setting: Power up PLL, P=1 and R=2
AIC3204_rset( 13, 0x00 );
// Hi_Byte(DOSR) for DOSR = 128 decimal or 0x0080 DAC oversamppling
AIC3204_rset( 14, 0x80 );
// Lo_Byte(DOSR) for DOSR = 128 decimal or 0x0080
AIC3204_rset( 20, 0x80 );
// AOSR for AOSR = 128 decimal or 0x0080 for decimation filters 1 to 6
AIC3204_rset( 11, 0x88 );
// Power up NDAC and set NDAC value to 8
AIC3204_rset( 12, 0x82 );
// Power up MDAC and set MDAC value to 2
AIC3204_rset( 18, 0x88 );
// Power up NADC and set NADC value to 8
AIC3204_rset( 19, 0x82 );
// Power up MADC and set MADC value to 2
// DAC ROUTING and Power Up
AIC3204_rset( 0, 0x01 );
// Select page 1
AIC3204_rset( 12, 0x08 );
// LDAC AFIR routed to HPL
AIC3204_rset( 13, 0x08 );
// RDAC AFIR routed to HPR
AIC3204_rset( 0, 0x00 );
// Select page 0
AIC3204_rset( 64, 0x02 );
// Left vol=right vol
AIC3204_rset( 65, 0x00 );
// Left DAC gain to 0dB VOL; Right tracks Left
AIC3204_rset( 63, 0xd4 );
// Power up left,right data paths and set channel
AIC3204_rset( 0, 0x01 );
// Select page 1
AIC3204_rset( 16, 0x06 );
// Unmute HPL , 6dB gain
AIC3204_rset( 17, 0x06);
// Unmute HPR , 6dB gain
AIC3204_rset( 9, 0x30 );
// Power up HPL,HPR
AIC3204_rset( 0, 0x00 );
// Select page 0
wait( 500 );
// Wait
// ADC ROUTING and Power Up
AIC3204_rset( 0, 0x01 );
// Select page 1
AIC3204_rset( 52, 0x00 );
// STEREO 1 Jack
// IN1_L not routing to LADC_P
AIC3204_rset( 55, 0xC0 );
// IN1_R to RADC_P through 40 kohmm
AIC3204_rset( 54, 0x03 );
// CM_1 (common mode) to LADC_M through 40 kohm
AIC3204_rset( 57, 0xC0 );
// CM_1 (common mode) to RADC_M through 40 kohm
AIC3204_rset( 59, 0x0f );
// MIC_PGA_L unmute
AIC3204_rset( 60, 0x0f );
// MIC_PGA_R unmute
AIC3204_rset( 0, 0x00 );
// Select page 0
AIC3204_rset( 81, 0xc0 );
// Powerup Left and Right ADC
AIC3204_rset( 82, 0x00 );
// Unmute Left and Right ADC
AIC3204_rset( 0, 0x00 );
wait( 200 );
// Wait
And configured I2S2 as:
void
Init_I2S2(void)
{
//I2S2_SRATE = 0x0015; //FS divider by 32 and CLK by 64
I2S2_SRATE = 0x0014;
//FS divider by 32 and CLK by 32
I2S2_INTMASK = 0x0028;
I2S2_SCTRL = 0x8012;
//Enable I2S, Stereo Mode, 16bit word and Master mode
}
I can see WS and BCLK as I want. However DX and RX are not sending nothing. I have an audio signal in IN1R.
I have tested it in EVM5515 and is working. The only difference that i see is that in EVM seems like if there is a pull up in DX, however i can't see anyone in schematics.
It is necessary a pull up in DX?
Thanks